ZPS_eAplAfGetNodePowerDescriptor

ZPS\_teStatus ZPS\_eAplAfGetNodePowerDescriptor\(
            ZPS\_tsAplAfNodePowerDescriptor *psDesc);

Description

This function copies the Node Power descriptor (for the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).

Parent topic:ZPS_eAplAfGetNodePowerDescriptor

Parameters

* psDesc Pointer to structure (see Section 8.2.1.2) to receive Node Power descriptor

Parent topic:ZPS_eAplAfGetNodePowerDescriptor

Returns

Parent topic:ZPS_eAplAfGetNodePowerDescriptor

Parent topic:Descriptor functions