ZPS_eAplAfGetSimpleDescriptor

ZPS\_teStatus ZPS\_eAplAfGetSimpleDescriptor\(
        uint8 u8Endpoint,
        ZPS\_tsAplAfSimpleDescriptor *psDesc);

Description

This function copies the Simple descriptor for the specified endpoint (on the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).

Parent topic:ZPS_eAplAfGetSimpleDescriptor

Parameters

* psDesc Pointer to structure (see Section 8.2.1.3) to receive Simple descriptor

Parent topic:ZPS_eAplAfGetSimpleDescriptor

Returns

Parent topic:ZPS_eAplAfGetSimpleDescriptor

Parent topic:Descriptor functions