ZPS_eAplAfInit
ZPS_teStatus ZPS_eAplAfInit(void);
Description
This function initializes the Application Framework and must be the first network function called in your application code. The function first requests a reset of the Network (NWK) layer of the ZigBee PRO stack. It then initializes certain network parameters with values that have been pre-configured using the ZPS Configuration Editor (see Chapter 13, ZPS Configuration Editor). These parameters include the node type and the Extended PAN ID of the network.
The device is started as the pre-configured node type. If this is a Coordinator, the Extended PAN ID of the node is set to the pre-configured value. Note that if a zero value is specified, the Coordinator uses its own IEEE/MAC address for the Extended PAN ID.
Parent topic:ZPS_eAplAfInit
Parameters
None.
Parent topic:ZPS_eAplAfInit
Returns
ZPS_E_SUCCESS (AF successfully initialized).
APS return codes, listed and described in Section 11.2.2.
NWK return codes, listed and described in Section 11.2.3.
MAC return codes, listed and described in Section 11.2.4.
Parent topic:ZPS_eAplAfInit
Parent topic:initialization functions