ZPS_eAplZdpDeviceAnnceRequest
ZPS_teStatus ZPS_eAplZdpDeviceAnnceRequest(
PDUM_thAPduInstance hAPduInst,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpDeviceAnnceReq *psZdpDeviceAnnceReq);
Description
This function is used to notify other nodes that the local node has joined or rejoined the network. The function broadcasts a Device_annce announcement to the network and is normally automatically called by the ZDO when the local node joins or rejoins the network.
The IEEE (MAC) and allocated network addresses as well as the capabilities of the sending node must be specified in the announcement, represented by the structure below (detailed further in Section 9.2.2.3).
typedef struct {
uint16 u16NwkAddr;
uint64 u64IeeeAddr;
uint8 u8Capability;
} ZPS_tsAplZdpDeviceAnnceReq;
On receiving this announcement, a network node updates any information it holds that relates to the supplied IEEE and network addresses:
If it already holds the supplied IEEE address, it updates the corresponding network address with the supplied one (if necessary).
If it already holds the supplied network address but with a different corresponding IEEE address, the latter is marked as not having a valid corresponding network address.
Parent topic:ZPS_eAplZdpDeviceAnnceRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent
* pu8SeqNumber Pointer to sequence number of announcement
* psZdpDeviceAnnceReq Pointer to announcement (see above)
Parent topic:ZPS_eAplZdpDeviceAnnceRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpDeviceAnnceRequest
Parent topic:Address discovery functions