rtc_func_peripheral#
Overview#
The RTC demo application demonstrates the important features of the RTC Module by using the RTC Peripheral Driver.
The RTC demo supports the following features:
Calendar
Get the current date time with Year, Month, Day, Hour, Minute, and Second.
Set the current date time with Year, Month, Day, Hour, Minute, and Second.
Alarm
Set the alarm based on the current time.
Application prints a notification when the alarm expires.
Seconds interrupt
Use second interrupt function to display a digital time blink every second.
Supported Boards#
FRDM-K22F
Hardware requirements
Mini/micro USB cable
FRDM-K22F board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following menu is displayed in the serial terminal:
RTC Peripheral Demo running...
Please choose the sub demo to run:
1) Get current date time.
2) Set current date time.
3) Alarm trigger show.
4) Second interrupt show (demo for 20s).
Select:
Get current date time:
This command gets the current date time in the format of YYYY-MM-DD HH:MM:SS.
Current datetime: 2015-11-11 11:11:11
Set current date time
Sets the date time as YYYY-MM-DD HH:MM:SS.
Input date time like: "2010-10-10 10:10:10"
2009-10-10 10:10:10
Show the alarm function
Sets the alarm time: 1~9 seconds from the time you input and waits for the alarm event arrival.
Input the alarm seconds from the current moment (1s~9s):3
Triggered Alarm: 10:10:31
Seconds interrupt show
Shows the digital time animation by seconds-interrupt function.
10:10:51
10:10:51
...
10:11:11
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following menu is displayed on the serial terminal:
RTC Peripheral Demo running...
Please choose the sub demo to run:
1) Get current date time.
2) Set current date time.
3) Alarm trigger show.
4) Second interrupt show (demo for 20s).
Select:
Get current date time:
This command gets the current date time in the format of YYYY-MM-DD HH:MM:SS.
Current datetime: 2016-11-11 11:11:11
Set current date time
Sets the date time as YYYY-MM-DD HH:MM:SS.
Input date time like: "2010-10-10 10:10:10"
2009-10-10 10:10:10
Show the alarm function
Sets the alarm time: 1~9 seconds from the time you input and waits for the alarm event arrival.
Input the alarm seconds from the current moment (1s~9s):3
Triggered Alarm: 10:10:31
Seconds interrupt show
Shows the digital time animation by seconds-interrupt function.
10:10:51
10:10:52
...
10:11:11
FRDM-MCXC242
Hardware requirements
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following menu is displayed in the serial terminal:
RTC Peripheral Demo running...
Please choose the sub demo to run:
1) Get current date time.
2) Set current date time.
3) Alarm trigger show.
4) Second interrupt show (demo for 20s).
Select:
Get current date time:
This command gets the current date time in the format of YYYY-MM-DD HH:MM:SS.
Current datetime: 2015-11-11 11:11:11
Set current date time
Sets the date time as YYYY-MM-DD HH:MM:SS.
Input date time like: "2010-10-10 10:10:10"
2009-10-10 10:10:10
Show the alarm function
Sets the alarm time: 1~9 seconds from the time you input and waits for the alarm event arrival.
Input the alarm seconds from the current moment (1s~9s):3
Triggered Alarm: 10:10:31
Seconds interrupt show
Shows the digital time animation by seconds-interrupt function.
10:10:51
10:10:51
...
10:11:11