multi_peripherals_test

Overview

The multi-peripherals-test demo application does the basic peripheral test on board. This demo will test audio, usb, led, button, sdcard, accelerometer and rtc. To test audio function, connect an audio source, for example from a mobile phone or PC, to Line-IN connector, connect a headphone or speaker to Line-Out connector. Then the input audio can be heared in the headphone or speaker. To test usb, connect a USB cable between the PC and board’s high speed connector, the cursor on the PC will move in a square pattern. To test sdcard function, insert a uSD memory card in to the connector, then the test result will be printed, please make sure the message is not a failed message. Please verify the green LED in the RGB-LED flashed with a 1Hz rate. This indicates that the RTC crystal works.

Supported Boards