peripheral_ipsp
Overview
Application demonstrating the BLE Peripheral role, except that this application specifically exposes the Internet Protocol Support GATT Service.
Prepare the Demo
Open example’s project and build it.
Connect a USB cable between the PC host and the OpenSDA USB port on the target board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
The demo does not require user interaction. The application will automatically start advertising the IPSP Service and it will accept the first connection request it receives. The application will perform the required setup for the L2CAP credit-based channel specified by the IPSP Profile. The application will display in console any message it receives from the peer through the L2CAP channel. Example output:
Received message: hello
Received message: hello
Received message: hello