unicast_media_sender#
Overview#
Application demonstrating how to use the unicast media sender feature.
There should be three boards: 1 UMS + 1 UMR(left) + 1 UMR(right).
UMS: unicast stereo audio stream, left channel on first CIS and right channel on another CIS.
UMR: receive one of CIS channel and render it.
Prepare the Demo#
Open example’s project and build it.
Connect a USB cable between the PC host and the OpenSDA USB port on the target board.
Provide 5V voltage for the target board.
Save a wav music file to a USB disk’s root directory and named as “music_16_2.wav”.
Connect the USB disk to USB OTG port.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
The log below shows the output of the example in the terminal window.
Copyright 2024 NXP
UMS>>
Unicast Media Sender.
Initializing
Initialized
wav file list:
1, 1:/._music_8000_2ch_16bits.wav
2, 1:/music_48000_2ch_16bits.wav
3, 1:/._music_16_2.wav
4, 1:/music_44100_2ch_16bits.wav
5, 1:/music_32000_2ch_16bits.wav
6, 1:/play_1ksin_48k_16b.wav
7, 1:/music_24000_2ch_16bits.wav
8, 1:/music_16000_2ch_16bits.wav
9, 1:/music_8000_2ch_16bits.wav
10, 1:/music_16_2.wav
11, 1:/sine_16_2.wav
12, 1:/sine_8000_2ch_16bits.wav
13, 1:/sine_16000_2ch_16bits.wav
14, 1:/sine_24000_2ch_16bits.wav
15, 1:/sine_32000_2ch_16bits.wav
16, 1:/sine_44100_2ch_16bits.wav
17, 1:/sine_48000_2ch_16bits.wav
18, 1:/sine_16000_2ch_32bits.wav
19, 1:/sine_16000_2ch_24bits.wav
20, 1:/sine_8000_2ch_16bits_0_75.wav
21, 1:/sine_16000_2ch_16bits_0_75.wav
22, 1:/sine_32000_2ch_16bits_0_75.wav
23, 1:/sine_48000_2ch_16bits_0_75.wav
24, 1:/chrip_48000_2ch_16bits_0_80.wav
25, 1:/play_1ksin_8k_16b.wav
26, 1:/play_1ksin_32k_16b.wav
wav file list complete!
Please open the wav file you want use "wav_open <path>" command.
UMS>>
UMS>>
UMS>> wav_open 1:/music_16_2.wav
wav file info:
UMS>> sample_rate: 16000
channels: 2
bits: 16
size: 3827552
samples: 956888
Please select lc3 preset use "lc3_preset <name>" command.
UMS>>
UMS>>
UMS>> lc3_preset 16_2_1
16_2_1:
codec_cfg - sample_rate: 16000, duration: 10000, len: 40
qos - interval: 10000, framing: 0, phy: 2, sdu: 40, rtn: 2, pd: 40000
UMS>> LC3 encoder setup done!
Creating unicast group
Unicast group created
Please scan and connect the devices you want!
UMS>>
UMS>>
UMS>> scan
Scanning successfully started
UMS>>
UMS>>
UMS>> [0]: CC:F8:26:ED:E7:82 (public), rssi -55, Galaxy Buds2 Pro
[1]: CC:F8:26:F6:87:8C (public), rssi -52, Galaxy Buds2 Pro
connect 0
UMS>> device selected!
Connecting
Connect first device
MTU exchanged: 23/23
LE Connected: CC:F8:26:ED:E7:82 (public)
MTU exchanged: 196/196
Connected
CSIP discover
CSIP conn 202DC9F0 discovered set count 1
set 1/1 info:
sirk: cc f8 26 f6 87 8c cc f8 26 ed e7 82 cc f8 26 f6
set_size: 2
rank: 2
lockable: 1
CSIP discovered
Scan another member
member: CC:F8:26:F6:87:8C (public), rssi -48, Galaxy Buds2 Pro
Member discovered
Connecting
Connect second device
MTU exchanged: 23/23
LE Connected: CC:F8:26:F6:87:8C (public)
MTU exchanged: 196/196
Connected
CSIP discover
CSIP conn 202DCAEC discovered set count 1
set 1/1 info:
sirk: cc f8 26 f6 87 8c cc f8 26 ed e7 82 cc f8 26 f6
set_size: 2
rank: 1
lockable: 1
CSIP discovered
Discover VCS
VCS discover finished
Discover VCS complete.
Discovering sinks
codec_cap 2000A19C dir 0x01
codec id 0x06 cid 0x0000 vid 0x0000 count 19
data: type 0x01 value_len 2
b400
data: type 0x02 value_len 1
03
data: type 0x03 value_len 1
01
data: type 0x04 value_len 4
1a009b00
data: type 0x05 value_len 1
01
meta: type 0x01 value_len 2
0700
dir 1 loc 401
snk ctx 4095 src ctx 623
Sink #0: ep 202D9538
Sink #0: ep 202D9600
Discover sinks complete: err 0
Sinks discovered
Configuring streams
Audio Stream 202F26F4 configured
Configured sink stream[0]
Stream configured
Setting stream QoS
QoS: waiting for 0 streams
Audio Stream 202F26F4 QoS set
Stream QoS Set
Enabling streams
Audio Stream 202F26F4 enabled
Streams enabled
Starting streams
Audio Stream 202F26F4 started
Streams started
Discover VCS
VCS discover finished
Discover VCS complete.
Discovering sinks
codec_cap 2000A19C dir 0x01
codec id 0x06 cid 0x0000 vid 0x0000 count 19
data: type 0x01 value_len 2
b400
data: type 0x02 value_len 1
03
data: type 0x03 value_len 1
01
data: type 0x04 value_len 4
1a009b00
data: type 0x05 value_len 1
01
meta: type 0x01 value_len 2
0700
dir 1 loc 802
snk ctx 4095 src ctx 623
Sink #1: ep 202D99B0
Sink #1: ep 202D9A78
Discover sinks complete: err 0
Sinks discovered
Configuring streams
Audio Stream 202F2718 configured
Configured sink stream[1]
Stream configured
Setting stream QoS
QoS: waiting for 1 streams
Audio Stream 202F2718 QoS set
Stream QoS Set
Enabling streams
snk ctx 4091 src ctx 623
Audio Stream 202F2718 enabled
Streams enabled
Starting streams
Audio Stream 202F2718 started
Streams started
Procedures to run
input “help” to show command list.
make sure UMR left and right are initialized and start advertising.
input “wav_open
” to open one wav file. input “lc3_preset
” to load one lc3 preset. input “scan” to start scan all sink devices, then use “connect” to connect one of the set member. Another set member will be connected automatically.
the audio will start playing after all config done.
input “pause” to stop playing.
input “play” to start playing.
input “vol_up”, “vol_down”, “vol_set” to set volume of all sinks.
input “vol_mute”, “vol_unmute” to set mute of all sinks.
Note:
“exit” command is a shell internal command, only used to exit shell module and could not used to exit demo.
the “music_16_2.wav” should be 16/24/32bits 2 channel with sample rate 8000/16000/24000/32000/48000.
Other cmds could be used:
“lc3_preset_list” used to list all the lc3 preset this demo support.
“sync_info” used to get iso_interval/sync_delay, and this cmd should be used after the audio stream start.
“config_rtn” used to config the rtn, and this cmd should be used before “lc3_preset”.
“config_pd” used to config the pd, and this cmd should be used before “lc3_preset”.
“config_phy” used to config the phy, and this cmd should be used before “lc3_preset”.
“config_packing” used to config iso packing mode, and this cmd should be used before “lc3_preset”.