MCUXpresso SDK Documentation

vg_lite_path_t structure

vg_lite_path_t structure#

This structure describes VGLite path data.

Path data is made of op codes and coordinates. The format for op codes is always VG_LITE_S8. For more details on opcodes, see Vector path opcodes for plotting paths.

Used in init functions: vg_lite_init_path, vg_lite_init_arc_path, vg_lite_upload_path, vg_lite_clear_path, vg_lite_append_path.

Used in draw functions: vg_lite_draw, vg_lite_draw_grad, vg_lite_draw_radial_grad, vg_lite_draw_pattern.

vg_lite_path_t members

Type

Description

bounding_box[4]

vg_lite_float_t

bounding box for path [0] left [1] top [2] right [3] bottom

quality

vg_lite_quality_t

enum for quality hint for the path, anti-aliasing level

format

vg_lite_format_t

enum for coordinate format

uploaded

vg_lite_hw_memory_t

struct with path data that has been uploaded into GPU addressable memory

path_length

vg_lite_uint32_t

number of bytes in the path

path

vg_lite_pointer

pointer to path data

path_changed

vg_lite_int8_t

0: not changed; 1: changed.

pdata_internal

vg_lite_int8_t

0: path data memory is allocated by application; 1: path data memory is allocated by driver.

path_type

vg_lite_path_type_t

The draw path type as specified in enum vg_lite_path_type_t. (added for stroke control, from March 2022)

*stroke

vg_lite_stroke_t

As defined by structure vg_lite_stroke_t (added for stroke control, from March 2022)

stroke_path

vg_lite_pointer

Pointer to the physical description of the stroke path. (added for stroke control, from March 2022)

stroke_size

vg_lite_uint32_t

Number of bytes in the stroke path data. (added for stroke control, from March 2022)

stroke_color

vg_lite_color_t

The stroke path fill color. (from Sept 2022)

add_end

vg_lite_int8_t

Flag that add end_path in driver (from March 2023)

Special notes for path objects:

  • Endianness has no impact, as it is aligned against the boundaries

  • Multiple contiguous opcodes should be packed by the size of the specified data format. For example, by 2 bytes for VG_LITE_S16 or by 4 bytes for VG_LITE_S32.

For example, because opcodes are 8-bit (1-byte), 16-bit (2-byte), or 32-bit (4-byte) data types:

…
<opcode1_that_needs_data>
<align_to_data_size>
<data_for_opcode1>
<opcode2_that_doesnt_need_data>
<align_to_data_size>
<opcode3_that_needs_data>
<align_to_data_size>
<data_for_opcode3>
…
  • Path data in the array should always be 1-, 2-, or 4-byte aligned, depending on the format:

For example, for 32-bit (4-byte) data types:

…
<opcode1_that_needs_data>
<pad to 4 bytes>
<4 byte data_for_opcode1>
<opcode2_that_doesnt_need_data>
<pad to 4 bytes>
<opcode3_that_needs_data>
<pad to 4 bytes>
<4 byte data_for_opcode3>
…

Parent topic:Vector path structures