Bluetooth Low Energy applications

The Software Development Package provides a Bluetooth Low Energy v5.3-compliant host stack implementation with a set of GATT-based profiles and services implemented on top. To demonstrate the device functionality, the following demo applications are implemented.

  1. ANCS Client

  2. Beacon Application

  3. Bluetooth LE FSCI Black Box

  4. EATT Central

  5. EATT Peripheral

  6. HCI Black Box

  7. HID Host

  8. HID Device (Mouse)

  9. Low-power Temperature Sensor and Collector

  10. Low-power Extended Advertising Central and Peripheral

  11. OTAP Clients ATT and L2CAP and OTAP Server

  12. Wireless UART demo application

  13. Bluetooth LE Shell application

  14. Hybrid (Dual-Mode) Bluetooth Low Energy and Generic FSK

Note: Refer to the application notes that are located in the ‘documentation’ folder.