41 #include "Driver_USART.h" 63 pHandle->
pComm = pCommInstance;
73 return ((ARM_DRIVER_USART *)(pHandle->
pComm))->Control(pControl->
control, pControl->
arg);
78 return ((ARM_DRIVER_USART *)(pHandle->
pComm))->Send(pData, size);
83 return ((ARM_DRIVER_USART *)(pHandle->
pComm))->Receive(pData, size);
comm_interface_t commUART
int32_t COMM_UART_Config(comm_handle_t *pHandle, void *pConfigData)
int32_t COMM_UART_Send(comm_handle_t *pHandle, void *pData, uint32_t size)
int32_t COMM_UART_Init(comm_handle_t *pHandle, void *pCommInstance, COMM_Event_t event, void *pInitializeData)
#define COMM_INTERFACE_OK
Operation succeeded.
The comm_interface.h file describes the interface definition for the communication interface...
int32_t COMM_UART_Receive(comm_handle_t *pHandle, void *pData, uint32_t size)
int32_t COMM_UART_GetCapabilities(comm_handle_t *pHandle)
void(* COMM_Event_t)(uint32_t event)
int32_t COMM_UART_GetStatus(comm_handle_t *pHandle)