ISSDK  1.7
IoT Sensing Software Development Kit
Functions | Variables
diff_p_drv.c File Reference

The diff_p_drv.c file implements the diff_p functional interface. More...

#include "gpio_driver.h"
#include "diff_p_drv.h"
#include "systick_utils.h"
Include dependency graph for diff_p_drv.c:

Go to the source code of this file.

Functions

void DIFF_P_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void DIFF_P_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 
int32_t DIFF_P_SPI_Initialize (diff_p_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
 The interface function to initialize the sensor. More...
 
void DIFF_P_SPI_SetIdleTask (diff_p_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t DIFF_P_SPI_Configure (diff_p_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t DIFF_P_SPI_ReadData (diff_p_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t DIFF_P_SPI_DeInit (diff_p_spi_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
int32_t DIFF_P_I2C_Initialize (diff_p_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
 The interface function to initialize the sensor. More...
 
void DIFF_P_I2C_SetIdleTask (diff_p_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the I2C Idle Task. More...
 
int32_t DIFF_P_I2C_Configure (diff_p_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t DIFF_P_I2C_ReadData (diff_p_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t DIFF_P_I2C_DeInit (diff_p_i2c_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 

Variables

uint8_t diff_p_spiRead_CmdBuffer [DIFF_P_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t diff_p_spiRead_DataBuffer [DIFF_P_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t diff_p_spiWrite_CmdDataBuffer [DIFF_P_SPI_MAX_MSG_SIZE] = {0}
 

Detailed Description

The diff_p_drv.c file implements the diff_p functional interface.

Definition in file diff_p_drv.c.

Function Documentation

◆ DIFF_P_I2C_Configure()

int32_t DIFF_P_I2C_Configure ( diff_p_i2c_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after DIFF_P_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_I2C_Configure() returns the status.

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 372 of file diff_p_drv.c.

References diff_p_i2c_sensorhandle_t::deviceInfo, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_SBYB_ACTIVE, DIFF_P_CTRL_REG1_SBYB_MASK, DIFF_P_CTRL_REG1_SBYB_STANDBY, int32_t(), diff_p_i2c_sensorhandle_t::isInitialized, diff_p_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_Write(), diff_p_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_I2C_DeInit()

int32_t DIFF_P_I2C_DeInit ( diff_p_i2c_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after DIFF_P_I2C_Initialize() has been called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_I2C_DeInit() returns the status.

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle.

Definition at line 444 of file diff_p_drv.c.

References diff_p_i2c_sensorhandle_t::deviceInfo, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_RST_MASK, DIFF_P_CTRL_REG1_RST_RESET, int32_t(), diff_p_i2c_sensorhandle_t::isInitialized, diff_p_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, diff_p_i2c_sensorhandle_t::slaveAddress, and status.

Here is the call graph for this function:

◆ DIFF_P_I2C_Initialize()

int32_t DIFF_P_I2C_Initialize ( diff_p_i2c_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
uint8_t  whoAmi 
)

The interface function to initialize the sensor.

This function initialize the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_I2C_Initialize() returns the status.

Check the input parameters.

Read and store the device's WHO_AM_I.

Initialize the sensor handle.

Put the device into standby mode so that we can run calibration can be done.

Run Calibration algorithm.

Wait for calibration to finish.

Definition at line 292 of file diff_p_drv.c.

References BOARD_DELAY_ms(), diff_p_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_SBYB_MASK, DIFF_P_CTRL_REG1_SBYB_STANDBY, DIFF_P_CTRL_REG2, DIFF_P_CTRL_REG2_CTRL_AC_CALRUN, DIFF_P_CTRL_REG2_CTRL_AC_MASK, DIFF_P_STATUS, DIFF_P_STATUS_STAT_EP_MASK, DIFF_P_WHO_AM_I, registerDeviceInfo_t::functionParam, registerDeviceInfo_t::idleFunction, int32_t(), diff_p_i2c_sensorhandle_t::isInitialized, diff_p_i2c_sensorhandle_t::pCommDrv, Register_I2C_Read(), Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, diff_p_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_I2C_ReadData()

int32_t DIFF_P_I2C_ReadData ( diff_p_i2c_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called only after DIFF_P_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_I2C_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 415 of file diff_p_drv.c.

References diff_p_i2c_sensorhandle_t::deviceInfo, int32_t(), diff_p_i2c_sensorhandle_t::isInitialized, diff_p_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_I2C_Read(), diff_p_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_I2C_SetIdleTask()

void DIFF_P_I2C_SetIdleTask ( diff_p_i2c_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the I2C Idle Task.

Parameters
[in]diff_p_i2c_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on I2C Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after DIFF_P_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 366 of file diff_p_drv.c.

References diff_p_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ DIFF_P_SPI_Configure()

int32_t DIFF_P_SPI_Configure ( diff_p_spi_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after DIFF_P_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_SPI_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 189 of file diff_p_drv.c.

References diff_p_spi_sensorhandle_t::deviceInfo, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_SBYB_ACTIVE, DIFF_P_CTRL_REG1_SBYB_MASK, DIFF_P_CTRL_REG1_SBYB_STANDBY, int32_t(), diff_p_spi_sensorhandle_t::isInitialized, diff_p_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_Write(), diff_p_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_SPI_DeInit()

int32_t DIFF_P_SPI_DeInit ( diff_p_spi_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after after DIFF_P_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
::DIFF_P_SPI_Deinit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle.

Definition at line 261 of file diff_p_drv.c.

References diff_p_spi_sensorhandle_t::deviceInfo, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_RST_MASK, DIFF_P_CTRL_REG1_RST_RESET, int32_t(), diff_p_spi_sensorhandle_t::isInitialized, diff_p_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, diff_p_spi_sensorhandle_t::slaveParams, and status.

Here is the call graph for this function:

◆ DIFF_P_SPI_Initialize()

int32_t DIFF_P_SPI_Initialize ( diff_p_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSlaveSelect,
uint8_t  whoAmi 
)

The interface function to initialize the sensor.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Read and store the device's WHO_AM_I.

Put the device into standby mode so that we can run calibration can be done.

Run Calibration algorithm.

Wait for calibration to finish.

Definition at line 92 of file diff_p_drv.c.

References BOARD_DELAY_ms(), GENERIC_DRIVER_GPIO::clr_pin, diff_p_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, DIFF_P_CTRL_REG1, DIFF_P_CTRL_REG1_SBYB_MASK, DIFF_P_CTRL_REG1_SBYB_STANDBY, DIFF_P_CTRL_REG2, DIFF_P_CTRL_REG2_CTRL_AC_CALRUN, DIFF_P_CTRL_REG2_CTRL_AC_MASK, DIFF_P_SPI_CMD_LEN, DIFF_P_SPI_ReadPreprocess(), DIFF_P_SPI_WritePreprocess(), DIFF_P_SS_ACTIVE_VALUE, DIFF_P_STATUS, DIFF_P_STATUS_STAT_EP_MASK, DIFF_P_WHO_AM_I, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), diff_p_spi_sensorhandle_t::isInitialized, diff_p_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, Register_SPI_Read(), Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, GENERIC_DRIVER_GPIO::set_pin, diff_p_spi_sensorhandle_t::slaveParams, SPI_SS_ACTIVE_LOW, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_SPI_ReadData()

int32_t DIFF_P_SPI_ReadData ( diff_p_spi_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after DIFF_P_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
DIFF_P_SPI_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 232 of file diff_p_drv.c.

References diff_p_spi_sensorhandle_t::deviceInfo, int32_t(), diff_p_spi_sensorhandle_t::isInitialized, diff_p_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_SPI_Read(), diff_p_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ DIFF_P_SPI_ReadPreprocess()

void DIFF_P_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 57 of file diff_p_drv.c.

References DIFF_P_SPI_CMD_LEN, diff_p_spiRead_CmdBuffer, diff_p_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by DIFF_P_SPI_Initialize().

Here is the caller graph for this function:

◆ DIFF_P_SPI_SetIdleTask()

void DIFF_P_SPI_SetIdleTask ( diff_p_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]diff_p_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after DIFF_P_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 183 of file diff_p_drv.c.

References diff_p_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ DIFF_P_SPI_WritePreprocess()

void DIFF_P_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 73 of file diff_p_drv.c.

References DIFF_P_SPI_CMD_LEN, diff_p_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by DIFF_P_SPI_Initialize().

Here is the caller graph for this function:

Variable Documentation

◆ diff_p_spiRead_CmdBuffer

uint8_t diff_p_spiRead_CmdBuffer[DIFF_P_SPI_MAX_MSG_SIZE] = {0}

Definition at line 50 of file diff_p_drv.c.

Referenced by DIFF_P_SPI_ReadPreprocess().

◆ diff_p_spiRead_DataBuffer

uint8_t diff_p_spiRead_DataBuffer[DIFF_P_SPI_MAX_MSG_SIZE] = {0}

Definition at line 51 of file diff_p_drv.c.

Referenced by DIFF_P_SPI_ReadPreprocess().

◆ diff_p_spiWrite_CmdDataBuffer

uint8_t diff_p_spiWrite_CmdDataBuffer[DIFF_P_SPI_MAX_MSG_SIZE] = {0}

Definition at line 52 of file diff_p_drv.c.

Referenced by DIFF_P_SPI_WritePreprocess().