![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_k22f.c file defines GPIO pins for FRDM-K22F board. More...
#include "frdm_k22f.h"
Go to the source code of this file.
Functions | |
| uint32_t | UART0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | DSPI0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | DSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The frdm_k22f.c file defines GPIO pins for FRDM-K22F board.
Definition in file frdm_k22f.c.
| uint32_t DSPI0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 312 of file frdm_k22f.c.
| uint32_t DSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 324 of file frdm_k22f.c.
| uint32_t I2C0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 288 of file frdm_k22f.c.
| uint32_t I2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 300 of file frdm_k22f.c.
| uint32_t UART0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 252 of file frdm_k22f.c.
| uint32_t UART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 264 of file frdm_k22f.c.
| uint32_t UART2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 276 of file frdm_k22f.c.
Definition at line 97 of file frdm_k22f.c.
Definition at line 104 of file frdm_k22f.c.
Definition at line 111 of file frdm_k22f.c.
Definition at line 118 of file frdm_k22f.c.
Definition at line 49 of file frdm_k22f.c.
Definition at line 42 of file frdm_k22f.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 221 of file frdm_k22f.c.
Definition at line 127 of file frdm_k22f.c.
Definition at line 134 of file frdm_k22f.c.
| gpioHandleKSDK_t D10 |
Definition at line 198 of file frdm_k22f.c.
| gpioHandleKSDK_t D11 |
Definition at line 65 of file frdm_k22f.c.
| gpioHandleKSDK_t D12 |
Definition at line 72 of file frdm_k22f.c.
| gpioHandleKSDK_t D13 |
Definition at line 58 of file frdm_k22f.c.
| gpioHandleKSDK_t D14 |
Definition at line 81 of file frdm_k22f.c.
| gpioHandleKSDK_t D15 |
Definition at line 88 of file frdm_k22f.c.
Definition at line 142 of file frdm_k22f.c.
Definition at line 149 of file frdm_k22f.c.
Definition at line 156 of file frdm_k22f.c.
Definition at line 163 of file frdm_k22f.c.
Definition at line 170 of file frdm_k22f.c.
Definition at line 177 of file frdm_k22f.c.
Definition at line 184 of file frdm_k22f.c.
Definition at line 191 of file frdm_k22f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 214 of file frdm_k22f.c.
| gpioHandleKSDK_t INT1 |
Definition at line 230 of file frdm_k22f.c.
| gpioHandleKSDK_t INT2 |
Definition at line 237 of file frdm_k22f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 207 of file frdm_k22f.c.