47 .clockName = kCLOCK_PortB,
54 .clockName = kCLOCK_PortB,
63 .clockName = kCLOCK_PortD,
70 .clockName = kCLOCK_PortD,
77 .clockName = kCLOCK_PortD,
86 .clockName = kCLOCK_PortE,
93 .clockName = kCLOCK_PortE,
102 .clockName = kCLOCK_PortB,
109 .clockName = kCLOCK_PortB,
116 .clockName = kCLOCK_PortC,
123 .clockName = kCLOCK_PortC,
132 .clockName = kCLOCK_PortD,
139 .clockName = kCLOCK_PortD,
147 .clockName = kCLOCK_PortB,
154 .clockName = kCLOCK_PortA,
161 .clockName = kCLOCK_PortA,
168 .clockName = kCLOCK_PortB,
175 .clockName = kCLOCK_PortC,
182 .clockName = kCLOCK_PortC,
189 .clockName = kCLOCK_PortB,
196 .clockName = kCLOCK_PortA,
203 .clockName = kCLOCK_PortD,
212 .clockName = kCLOCK_PortA,
219 .clockName = kCLOCK_PortA,
226 .clockName = kCLOCK_PortD,
235 .clockName = kCLOCK_PortD,
242 .clockName = kCLOCK_PortD,
254 return CLOCK_GetFreq(UART0_CLK_SRC);
266 return CLOCK_GetFreq(UART1_CLK_SRC);
278 return CLOCK_GetFreq(UART2_CLK_SRC);
290 return CLOCK_GetFreq(I2C0_CLK_SRC);
302 return CLOCK_GetFreq(I2C1_CLK_SRC);
314 return CLOCK_GetBusClkFreq();
326 return CLOCK_GetBusClkFreq();
uint32_t DSPI0_GetFreq(void)
Determines the Clock Frequency feature.
The GPIO pin handle for KSDK.
uint32_t UART2_GetFreq(void)
Determines the Clock Frequency feature.
The frdm_k22f.h file defines GPIO pins for FRDM-K22F board.
gpioHandleKSDK_t GREEN_LED
uint32_t I2C1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t I2C0_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleKSDK_t BLUE_LED
uint32_t DSPI1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART0_GetFreq(void)
Determines the Clock Frequency feature.