48 .clockName = kCLOCK_PortE,
55 .clockName = kCLOCK_PortE,
64 .clockName = kCLOCK_PortC,
71 .clockName = kCLOCK_PortC,
80 .clockName = kCLOCK_PortD,
87 .clockName = kCLOCK_PortD,
94 .clockName = kCLOCK_PortD,
103 .clockName = kCLOCK_PortC,
110 .clockName = kCLOCK_PortC,
119 .clockName = kCLOCK_PortB,
126 .clockName = kCLOCK_PortB,
133 .clockName = kCLOCK_PortB,
140 .clockName = kCLOCK_PortB,
147 .clockName = kCLOCK_PortB,
154 .clockName = kCLOCK_PortA,
161 .clockName = kCLOCK_PortB,
168 .clockName = kCLOCK_PortA,
175 .clockName = kCLOCK_PortC,
182 .clockName = kCLOCK_PortC,
189 .clockName = kCLOCK_PortA,
196 .clockName = kCLOCK_PortC,
203 .clockName = kCLOCK_PortD,
212 .clockName = kCLOCK_PortB,
219 .clockName = kCLOCK_PortE,
226 .clockName = kCLOCK_PortB,
235 .clockName = kCLOCK_PortC,
242 .clockName = kCLOCK_PortC,
254 return CLOCK_GetFreq(UART0_CLK_SRC);
266 return CLOCK_GetFreq(UART1_CLK_SRC);
278 return CLOCK_GetFreq(UART2_CLK_SRC);
290 return CLOCK_GetFreq(UART3_CLK_SRC);
302 return CLOCK_GetFreq(UART4_CLK_SRC);
314 return CLOCK_GetFreq(UART5_CLK_SRC);
326 return CLOCK_GetFreq(I2C0_CLK_SRC);
338 return CLOCK_GetFreq(I2C1_CLK_SRC);
350 return CLOCK_GetFreq(I2C2_CLK_SRC);
362 return CLOCK_GetBusClkFreq();
374 return CLOCK_GetBusClkFreq();
386 return CLOCK_GetBusClkFreq();
uint32_t DSPI0_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART5_GetFreq(void)
Determines the Clock Frequency feature.
The GPIO pin handle for KSDK.
gpioHandleKSDK_t BLUE_LED
uint32_t DSPI1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t DSPI2_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t I2C2_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART2_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART3_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t I2C0_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleKSDK_t GREEN_LED
uint32_t I2C1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t UART0_GetFreq(void)
Determines the Clock Frequency feature.
The frdm_k64f.h file defines GPIO pin mappings for FRDM-K64F board.
uint32_t UART4_GetFreq(void)
Determines the Clock Frequency feature.