![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_kl27z.h file defines GPIO pins for FRDM-KL27Z board. More...
#include "pin_mux.h"#include "fsl_smc.h"#include "MKL27Z644.h"#include "RTE_Device.h"#include "gpio_driver.h"

Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN D15 |
| #define | I2C_S1_SDA_PIN D14 |
| #define | I2C_S1_DRIVER Driver_I2C0 |
| #define | I2C_S1_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | I2C_S2_SCL_PIN A5 |
| #define | I2C_S2_SDA_PIN A4 |
| #define | I2C_S2_DRIVER Driver_I2C1 |
| #define | I2C_S2_DEVICE_INDEX I2C1_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
| #define | I2C_BB_SCL_PIN D15 |
| #define | I2C_BB_SDA_PIN D14 |
| #define | I2C_BB_DRIVER Driver_I2C1 |
| #define | I2C_BB_DEVICE_INDEX I2C1_INDEX |
| #define | I2C_BB_SIGNAL_EVENT I2C1_SignalEvent_t |
| #define | SPI_S_SCLK D13 |
| #define | SPI_S_MOSI D11 |
| #define | SPI_S_MISO D12 |
| #define | SPI_S_DRIVER Driver_SPI0 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI0_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI0_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART0 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | HOST_B_DRIVER Driver_USART0 |
| #define | HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | MMA845x_I2C_ADDR 0x1D |
| #define | MMA845x_INT1 INT1 |
| #define | MMA845x_INT2 INT2 |
| #define | MAG3110_I2C_ADDR 0x0E |
| #define | GPIO_TYPE GPIOC |
| #define | GPIO_PORT_NUM PORTC_NUM |
| #define | ASK_USER_TO_RESUME(x) |
| #define | ADS_NVM_ADDR 0x0000F800 |
| start of the next to last 1K (sector size) of the 64K flash More... | |
| #define | FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
The frdm_kl27z.h file defines GPIO pins for FRDM-KL27Z board.
Definition in file frdm_kl27z.h.
| #define ADS_NVM_ADDR 0x0000F800 |
start of the next to last 1K (sector size) of the 64K flash
Definition at line 150 of file frdm_kl27z.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 139 of file frdm_kl27z.h.
| #define FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
Definition at line 151 of file frdm_kl27z.h.
| #define GPIO_PORT_NUM PORTC_NUM |
Definition at line 136 of file frdm_kl27z.h.
Referenced by PORTAE_IRQHandler(), PORTB_PORTC_IRQHandler(), PORTB_PORTC_PORTD_PORTE_IRQHandler(), and PORTBCD_IRQHandler().
| #define GPIO_TYPE GPIOC |
Definition at line 135 of file frdm_kl27z.h.
Referenced by PORTAE_IRQHandler(), PORTB_PORTC_IRQHandler(), PORTB_PORTC_PORTD_PORTE_IRQHandler(), and PORTBCD_IRQHandler().
| #define HOST_B_DRIVER Driver_USART0 |
Definition at line 122 of file frdm_kl27z.h.
| #define HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 123 of file frdm_kl27z.h.
| #define HOST_S_DRIVER Driver_USART0 |
Definition at line 118 of file frdm_kl27z.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 119 of file frdm_kl27z.h.
| #define I2C_BB_DEVICE_INDEX I2C1_INDEX |
Definition at line 105 of file frdm_kl27z.h.
| #define I2C_BB_DRIVER Driver_I2C1 |
Definition at line 104 of file frdm_kl27z.h.
| #define I2C_BB_SCL_PIN D15 |
Definition at line 102 of file frdm_kl27z.h.
| #define I2C_BB_SDA_PIN D14 |
Definition at line 103 of file frdm_kl27z.h.
| #define I2C_BB_SIGNAL_EVENT I2C1_SignalEvent_t |
Definition at line 106 of file frdm_kl27z.h.
| #define I2C_S1_DEVICE_INDEX I2C0_INDEX |
Definition at line 91 of file frdm_kl27z.h.
| #define I2C_S1_DRIVER Driver_I2C0 |
Definition at line 90 of file frdm_kl27z.h.
| #define I2C_S1_SCL_PIN D15 |
Definition at line 88 of file frdm_kl27z.h.
| #define I2C_S1_SDA_PIN D14 |
Definition at line 89 of file frdm_kl27z.h.
| #define I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 92 of file frdm_kl27z.h.
| #define I2C_S2_DEVICE_INDEX I2C1_INDEX |
Definition at line 98 of file frdm_kl27z.h.
| #define I2C_S2_DRIVER Driver_I2C1 |
Definition at line 97 of file frdm_kl27z.h.
| #define I2C_S2_SCL_PIN A5 |
Definition at line 95 of file frdm_kl27z.h.
| #define I2C_S2_SDA_PIN A4 |
Definition at line 96 of file frdm_kl27z.h.
| #define I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
Definition at line 99 of file frdm_kl27z.h.
| #define MAG3110_I2C_ADDR 0x0E |
Definition at line 131 of file frdm_kl27z.h.
| #define MMA845x_I2C_ADDR 0x1D |
Definition at line 126 of file frdm_kl27z.h.
| #define MMA845x_INT1 INT1 |
Definition at line 127 of file frdm_kl27z.h.
| #define MMA845x_INT2 INT2 |
Definition at line 128 of file frdm_kl27z.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 113 of file frdm_kl27z.h.
| #define SPI_S_DEVICE_INDEX SPI0_INDEX |
Definition at line 114 of file frdm_kl27z.h.
| #define SPI_S_DRIVER Driver_SPI0 |
Definition at line 112 of file frdm_kl27z.h.
| #define SPI_S_MISO D12 |
Definition at line 111 of file frdm_kl27z.h.
| #define SPI_S_MOSI D11 |
Definition at line 110 of file frdm_kl27z.h.
| #define SPI_S_SCLK D13 |
Definition at line 109 of file frdm_kl27z.h.
| #define SPI_S_SIGNAL_EVENT SPI0_SignalEvent_t |
Definition at line 115 of file frdm_kl27z.h.
Definition at line 121 of file frdm_k64f.c.
Definition at line 128 of file frdm_k64f.c.
Definition at line 135 of file frdm_k64f.c.
Definition at line 66 of file frdm_k64f.c.
Definition at line 59 of file frdm_k64f.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 221 of file frdm_k64f.c.
Definition at line 98 of file frdm_k64f.c.
Definition at line 105 of file frdm_k64f.c.
| gpioHandleKSDK_t D10 |
Definition at line 198 of file frdm_k64f.c.
| gpioHandleKSDK_t D11 |
Definition at line 82 of file frdm_k64f.c.
| gpioHandleKSDK_t D12 |
Definition at line 89 of file frdm_k64f.c.
| gpioHandleKSDK_t D13 |
Definition at line 75 of file frdm_k64f.c.
| gpioHandleKSDK_t D14 |
Definition at line 50 of file frdm_k64f.c.
| gpioHandleKSDK_t D15 |
Definition at line 43 of file frdm_k64f.c.
Definition at line 142 of file frdm_k64f.c.
Definition at line 156 of file frdm_k64f.c.
Definition at line 163 of file frdm_k64f.c.
Definition at line 170 of file frdm_k64f.c.
Definition at line 177 of file frdm_k64f.c.
Definition at line 184 of file frdm_k64f.c.
Definition at line 191 of file frdm_k64f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 214 of file frdm_k64f.c.
| gpioHandleKSDK_t INT1 |
Definition at line 230 of file frdm_k64f.c.
| gpioHandleKSDK_t INT2 |
Definition at line 237 of file frdm_k64f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 207 of file frdm_k64f.c.