40 #ifndef FXAS21002_DRV_H_    41 #define FXAS21002_DRV_H_    87 #define FXAS21002_GYRO_DATA_SIZE (0x06)     91 #define FXAS21002_SPI_MAX_MSG_SIZE (64)    95 #define FXAS21002_SPI_CMD_LEN (1)    99 #define FXAS21002_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW   117                                  ARM_DRIVER_I2C *pBus,
   184                                  ARM_DRIVER_SPI *pBus,
   264 #endif // FXAS21002_DRV_H_ The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
 
void FXAS21002_SPI_SetIdleTask(fxas21002_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
int32_t FXAS21002_SPI_Initialize(fxas21002_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
void FXAS21002_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
 
int32_t FXAS21002_I2C_Deinit(fxas21002_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
int32_t FXAS21002_I2C_Configure(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
The fxas21002.h contains the fxas21002 sensor register definitions and its bit mask. 
 
void FXAS21002_I2C_SetIdleTask(fxas21002_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
int32_t FXAS21002_I2C_ReadData(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
int32_t FXAS21002_SPI_ReadData(fxas21002_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
This structure defines the fxas21002 raw data buffer. 
 
This defines the sensor specific information for I2C. 
 
registerDeviceInfo_t deviceInfo
 
int32_t FXAS21002_SPI_Configure(fxas21002_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
 
ARM_DRIVER_SPI * pCommDrv
 
int32_t FXAS21002_SPI_Deinit(fxas21002_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
int32_t FXAS21002_I2C_Initialize(fxas21002_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
spiSlaveSpecificParams_t slaveParams
 
This defines the sensor specific information for SPI. 
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
This structure defines the device specific info required by register I/O. 
 
This structure defines the spi slave command format. 
 
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
 
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
 
ARM_DRIVER_I2C * pCommDrv
 
void FXAS21002_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
 
registerDeviceInfo_t deviceInfo