ISSDK  1.7
IoT Sensing Software Development Kit
Data Structures | Macros | Functions
fxls8471q_drv.h File Reference

The fxls8471q_drv.h file describes the fxls8471q driver interface and structures. More...

#include <stdint.h>
#include "fxls8471q.h"
#include "sensor_io_spi.h"
#include "register_io_spi.h"
Include dependency graph for fxls8471q_drv.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  fxls8471q_spi_sensorhandle_t
 This defines the sensor specific information for SPI. More...
 
struct  fxls8471q_acceldata_t
 This structure defines the fxls8471q raw data buffer. More...
 

Macros

#define FXLS8471Q_ACCEL_DATA_SIZE   (0x06) /* Size of the accel data*/
 The size of the FXLS8471Q accel data. More...
 
#define FXLS8471Q_SPI_MAX_MSG_SIZE   (64)
 The MAX size of SPI message. More...
 
#define FXLS8471Q_SPI_CMD_LEN   (2)
 The size of the Sensor specific SPI Header. More...
 
#define FXLS8471Q_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW
 Is the Slave Select Pin Active Low or High. More...
 

Functions

int32_t FXLS8471Q_SPI_Initialize (fxls8471q_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
 The interface function to initialize the sensor for I2C. More...
 
void FXLS8471Q_SPI_SetIdleTask (fxls8471q_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t FXLS8471Q_SPI_Configure (fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t FXLS8471Q_SPI_ReadData (fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXLS8471Q_SPI_Deinit (fxls8471q_spi_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
void FXLS8471Q_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void FXLS8471Q_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 

Detailed Description

The fxls8471q_drv.h file describes the fxls8471q driver interface and structures.

Definition in file fxls8471q_drv.h.

Macro Definition Documentation

◆ FXLS8471Q_ACCEL_DATA_SIZE

#define FXLS8471Q_ACCEL_DATA_SIZE   (0x06) /* Size of the accel data*/

The size of the FXLS8471Q accel data.

Definition at line 74 of file fxls8471q_drv.h.

Referenced by main().

◆ FXLS8471Q_SPI_CMD_LEN

#define FXLS8471Q_SPI_CMD_LEN   (2)

The size of the Sensor specific SPI Header.

Definition at line 82 of file fxls8471q_drv.h.

Referenced by FXLS8471Q_Init(), FXLS8471Q_SPI_Initialize(), FXLS8471Q_SPI_ReadPreprocess(), and FXLS8471Q_SPI_WritePreprocess().

◆ FXLS8471Q_SPI_MAX_MSG_SIZE

#define FXLS8471Q_SPI_MAX_MSG_SIZE   (64)

The MAX size of SPI message.

Definition at line 78 of file fxls8471q_drv.h.

◆ FXLS8471Q_SS_ACTIVE_VALUE

#define FXLS8471Q_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW

Is the Slave Select Pin Active Low or High.

Definition at line 86 of file fxls8471q_drv.h.

Referenced by FXLS8471Q_Init(), and FXLS8471Q_SPI_Initialize().

Function Documentation

◆ FXLS8471Q_SPI_Configure()

int32_t FXLS8471Q_SPI_Configure ( fxls8471q_spi_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after FXLS8471Q_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8471Q_SPI_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 153 of file fxls8471q_drv.c.

References fxls8471q_spi_sensorhandle_t::deviceInfo, FXLS8471Q_CTRL_REG1, FXLS8471Q_CTRL_REG1_MODE_ACTIVE, FXLS8471Q_CTRL_REG1_MODE_MASK, FXLS8471Q_CTRL_REG1_MODE_STANDBY, int32_t(), fxls8471q_spi_sensorhandle_t::isInitialized, fxls8471q_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_Write(), fxls8471q_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8471Q_SPI_Deinit()

int32_t FXLS8471Q_SPI_Deinit ( fxls8471q_spi_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after after FXLS8471Q_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8471Q_SPI_Deinit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

De-initialize sensor handle.

Definition at line 225 of file fxls8471q_drv.c.

References fxls8471q_spi_sensorhandle_t::isInitialized, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, and SENSOR_ERROR_NONE.

◆ FXLS8471Q_SPI_Initialize()

int32_t FXLS8471Q_SPI_Initialize ( fxls8471q_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSlaveSelect,
uint8_t  whoAmi 
)

The interface function to initialize the sensor for I2C.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8471Q_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Read and store the device's WHO_AM_I.

Definition at line 93 of file fxls8471q_drv.c.

References GENERIC_DRIVER_GPIO::clr_pin, fxls8471q_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, FXLS8471Q_SPI_CMD_LEN, FXLS8471Q_SPI_ReadPreprocess(), FXLS8471Q_SPI_WritePreprocess(), FXLS8471Q_SS_ACTIVE_VALUE, FXLS8471Q_WHO_AM_I, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), fxls8471q_spi_sensorhandle_t::isInitialized, fxls8471q_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, Register_SPI_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, GENERIC_DRIVER_GPIO::set_pin, fxls8471q_spi_sensorhandle_t::slaveParams, SPI_SS_ACTIVE_LOW, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8471Q_SPI_ReadData()

int32_t FXLS8471Q_SPI_ReadData ( fxls8471q_spi_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXLS8471Q_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8471Q_SPI_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 196 of file fxls8471q_drv.c.

References fxls8471q_spi_sensorhandle_t::deviceInfo, int32_t(), fxls8471q_spi_sensorhandle_t::isInitialized, fxls8471q_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_SPI_Read(), fxls8471q_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8471Q_SPI_ReadPreprocess()

void FXLS8471Q_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 56 of file fxls8471q_drv.c.

References FXLS8471Q_SPI_CMD_LEN, fxls8471q_spiRead_CmdBuffer, fxls8471q_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLS8471Q_Init(), and FXLS8471Q_SPI_Initialize().

Here is the caller graph for this function:

◆ FXLS8471Q_SPI_SetIdleTask()

void FXLS8471Q_SPI_SetIdleTask ( fxls8471q_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]fxls8471q_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXLS8471Q_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 145 of file fxls8471q_drv.c.

References fxls8471q_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXLS8471Q_SPI_WritePreprocess()

void FXLS8471Q_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 73 of file fxls8471q_drv.c.

References FXLS8471Q_SPI_CMD_LEN, fxls8471q_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLS8471Q_Init(), and FXLS8471Q_SPI_Initialize().

Here is the caller graph for this function: