![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The fxpq3115_oneshot.c file implements the ISSDK FXPQ3115BV sensor driver example demonstration with one-shot sampling mode. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "fxpq3115_drv.h"
Go to the source code of this file.
Macros | |
| #define | FXPQ3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | B3115ConfigAltitude [] |
| Register settings for Altitude readings in One-Shot mode. More... | |
| const registerwritelist_t | B3115SetOST [] |
| Register settings for Triggring One-Shot Sampling. More... | |
| const registerreadlist_t | B3115GetOST [] = {{.readFrom = FXPQ3115_CTRL_REG1, .numBytes = 1}, __END_READ_DATA__} |
| Address of Register containing OST Bit. More... | |
| const registerreadlist_t | B3115OutputNormal [] |
| Address and size of Raw Altitude+Temperature Data. More... | |
The fxpq3115_oneshot.c file implements the ISSDK FXPQ3115BV sensor driver example demonstration with one-shot sampling mode.
Definition in file fxpq3115_oneshot.c.
Definition at line 61 of file fxpq3115_oneshot.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize FXPQ3115 sensor driver.
We do not need to call FXPQ3115_I2C_Configure() in this case as we are going to read samples on demand. Instead we directly write register settings for One-Shot Mode...
The code contained withing the braces illustrate steps to read one-sample. These can be repated at desired intervals to acquire more samples.
Keep checking the OST FLAG for completion.
Read raw sensor data from the FXPQ3115.
Process the sample and convert the raw sensor data.
Definition at line 91 of file fxpq3115_oneshot.c.
References fxpq3115_altitudedata_t::altitude, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, PhysicalSensor::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, FXPQ3115_ALTITUDE_CONV_FACTOR, FXPQ3115_CTRL_REG1_OST_MASK, FXPQ3115_DATA_SIZE, FXPQ3115_I2C_ADDR, FXPQ3115_I2C_Initialize(), FXPQ3115_I2C_ReadData(), FXPQ3115_TEMPERATURE_CONV_FACTOR, FXPQ3115_WHOAMI_VALUE, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, registerDeviceInfo_t::idleFunction, int32_t(), fxpq3115_i2c_sensorhandle_t::pCommDrv, rawData, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_Write(), fxpq3115_i2c_sensorhandle_t::slaveAddress, SMC, SMC_SetPowerModeWait(), status, and fxpq3115_altitudedata_t::temperature.

| const registerwritelist_t B3115ConfigAltitude[] |
Register settings for Altitude readings in One-Shot mode.
Definition at line 67 of file fxpq3115_oneshot.c.
| const registerreadlist_t B3115GetOST[] = {{.readFrom = FXPQ3115_CTRL_REG1, .numBytes = 1}, __END_READ_DATA__} |
Address of Register containing OST Bit.
Definition at line 79 of file fxpq3115_oneshot.c.
| const registerreadlist_t B3115OutputNormal[] |
Address and size of Raw Altitude+Temperature Data.
Definition at line 82 of file fxpq3115_oneshot.c.
| const registerwritelist_t B3115SetOST[] |
Register settings for Triggring One-Shot Sampling.
Definition at line 73 of file fxpq3115_oneshot.c.