![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The pedometer_stepcount_fxos8700.c file implements the ISSDK prdometer example using FXOS8700 sensor as the acceleration source. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "pedometer.h"#include "fxos8700_drv.h"
Go to the source code of this file.
Macros | |
| #define | RAW_ACCEL_DATA_SIZE (6) |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | fxos8700_Config [] |
| const registerreadlist_t | FXOS8700_STATUS_READ [] = {{.readFrom = FXOS8700_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | FXOS8700_ACCEL_READ [] |
The pedometer_stepcount_fxos8700.c file implements the ISSDK prdometer example using FXOS8700 sensor as the acceleration source.
The pedometer_stepcount_fxos8700.c file implements the ISSDK FXOS8700 sensor driver example demonstration for Motion Activated Pedometer.
Definition in file pedometer_stepcount_fxos8700.c.
| #define RAW_ACCEL_DATA_SIZE (6) |
Definition at line 58 of file pedometer_stepcount_fxos8700.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the FXOS8700 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the fxos8700 sensor driver.
Definition at line 110 of file pedometer_stepcount_fxos8700.c.
References fxos8700_acceldata_t::accel, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), FXOS8700_I2C_ADDR, FXOS8700_I2C_Configure(), FXOS8700_I2C_Initialize(), FXOS8700_I2C_ReadData(), FXOS8700_I2C_SetIdleTask(), FXOS8700_WHO_AM_I_PROD_VALUE, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, int32_t(), pedometer_configure(), pedometer_init(), pedometer_run(), RAW_ACCEL_DATA_SIZE, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeWait(), pedometer_t::status, status, and pedometer_t::pedometer_status_tag::stepcount.

| const registerreadlist_t FXOS8700_ACCEL_READ[] |
Command definition to read the Accel Data
Definition at line 99 of file pedometer_stepcount_fxos8700.c.
| const registerwritelist_t fxos8700_Config[] |
Definition at line 66 of file pedometer_stepcount_fxos8700.c.
| const registerreadlist_t FXOS8700_STATUS_READ[] = {{.readFrom = FXOS8700_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Command definition to read the Data Ready Status
Definition at line 96 of file pedometer_stepcount_fxos8700.c.