14 #ifndef FXLS8471Q_DRV_H_    15 #define FXLS8471Q_DRV_H_    48 #define FXLS8471Q_ACCEL_DATA_SIZE (0x06)     52 #define FXLS8471Q_SPI_MAX_MSG_SIZE (64)    56 #define FXLS8471Q_SPI_CMD_LEN (2)    60 #define FXLS8471Q_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW   158 #endif // FXLS8471Q_DRV_H_ 
This defines the sensor specific information for SPI. 
 
int32_t FXLS8471Q_SPI_Initialize(fxls8471q_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
The interface function to initialize the sensor for I2C. 
 
This structure defines the device specific info required by register I/O. 
 
registerDeviceInfo_t deviceInfo
 
This structure defines the Write command List. 
 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
 
The fxls8471q.h file contains the register definitions for fxls8471q sensor driver. 
 
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
 
This structure defines the spi slave command format. 
 
int32_t FXLS8471Q_SPI_Deinit(fxls8471q_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
ARM_DRIVER_SPI * pCommDrv
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
This structure defines the fxls8471q raw data buffer. 
 
spiSlaveSpecificParams_t slaveParams
 
void FXLS8471Q_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
 
int32_t FXLS8471Q_SPI_ReadData(fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
int32_t FXLS8471Q_SPI_Configure(fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
void FXLS8471Q_SPI_SetIdleTask(fxls8471q_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
This structure defines the Read command List. 
 
void FXLS8471Q_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...