13 #ifndef FXLS896X_AF_H_    14 #define FXLS896X_AF_H_    60 #define FXLS896x_SPI_MAX_MSG_SIZE (64)    64 #define FXLS896x_SPI_CMD_LEN (2)    68 #define FXLS896x_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW   150                                 ARM_DRIVER_SPI *pBus,
   230 #endif // FXLS896X_AF_H_ 
This structure defines the device specific info required by register I/O. 
 
This structure defines the Write command List. 
 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
 
void FXLS896x_I2C_SetIdleTask(fxls896x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
ARM_DRIVER_SPI * pCommDrv
 
void FXLS896x_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
 
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
 
This structure defines the spi slave command format. 
 
This defines the sensor specific information for SPI. 
 
This file contains the FXLS896XAF Accelerometer register definitions, access macros, and device access functions. 
 
registerDeviceInfo_t deviceInfo
 
void FXLS896x_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
 
int32_t FXLS896x_SPI_Configure(fxls896x_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
void FXLS896x_SPI_SetIdleTask(fxls896x_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
int32_t FXLS896x_SPI_ReadData(fxls896x_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
This structure defines the fxls896x raw data buffer. 
 
int32_t FXLS896x_SPI_Initialize(fxls896x_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoAmi)
The interface function to initialize the sensor. 
 
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
This defines the sensor specific information for I2C. 
 
int32_t FXLS896x_SPI_Deinit(fxls896x_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
ARM_DRIVER_I2C * pCommDrv
 
registerDeviceInfo_t deviceInfo
 
int32_t FXLS896x_I2C_DeInit(fxls896x_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
int32_t FXLS896x_I2C_Initialize(fxls896x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoAmi)
The interface function to initialize the sensor. 
 
This structure defines the Read command List. 
 
int32_t FXLS896x_I2C_Configure(fxls896x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
spiSlaveSpecificParams_t slaveParams
 
int32_t FXLS896x_I2C_ReadData(fxls896x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...