13 #ifndef FXLS8974_DRV_H_ 14 #define FXLS8974_DRV_H_ 60 #define FXLS8974_SPI_MAX_MSG_SIZE (64) 64 #define FXLS8974_SPI_CMD_LEN (2) 68 #define FXLS8974_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW 150 ARM_DRIVER_SPI *pBus,
230 #endif // FXLS8974_DRV_H_
void FXLS8974_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.
This structure defines the device specific info required by register I/O.
This structure defines the Write command List.
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
void FXLS8974_SPI_SetIdleTask(fxls8974_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task.
spiSlaveSpecificParams_t slaveParams
int32_t FXLS8974_SPI_Initialize(fxls8974_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoAmi)
The interface function to initialize the sensor.
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
This structure defines the spi slave command format.
int32_t FXLS8974_I2C_ReadData(fxls8974_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
This defines the sensor specific information for I2C.
void FXLS8974_I2C_SetIdleTask(fxls8974_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
int32_t FXLS8974_SPI_ReadData(fxls8974_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
int32_t FXLS8974_SPI_Deinit(fxls8974_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor..
ARM_DRIVER_SPI * pCommDrv
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
int32_t FXLS8974_I2C_DeInit(fxls8974_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor..
This defines the sensor specific information for SPI.
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
This structure defines the fxls8974 raw data buffer.
int32_t FXLS8974_SPI_Configure(fxls8974_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
registerDeviceInfo_t deviceInfo
ARM_DRIVER_I2C * pCommDrv
void FXLS8974_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
This structure defines the Read command List.
int32_t FXLS8974_I2C_Initialize(fxls8974_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoAmi)
The interface function to initialize the sensor.
int32_t FXLS8974_I2C_Configure(fxls8974_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
registerDeviceInfo_t deviceInfo
The sensor_io_i2c.h file declares low-level interface functions for reading and writing sensor regist...
This file contains the FXLS8974CF Accelerometer register definitions, access macros, and device access functions.