![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Data Structures | |
| union | ISL29023_CMD_I_t |
| union | ISL29023_CMD_II_t |
Macros | |
| #define | ISL29023_I2C_ADDRESS (0x44) /*ISL29023 I2C Address */ |
| #define | ISL29023_I2C_TEST_VALUE (0x00) /*ISL29023 test register value */ |
| #define | ISL29023_CMD_I_PRST_MASK ((uint8_t) 0x03) |
| #define | ISL29023_CMD_I_PRST_SHIFT ((uint8_t) 0) |
| #define | ISL29023_CMD_I_FLAG_MASK ((uint8_t) 0x04) |
| #define | ISL29023_CMD_I_FLAG_SHIFT ((uint8_t) 2) |
| #define | ISL29023_CMD_I_OP_MASK ((uint8_t) 0xe0) |
| #define | ISL29023_CMD_I_OP_SHIFT ((uint8_t) 5) |
| #define | ISL29023_CMD_I_PRST_1 ((uint8_t) 0x00) /* Number of Integration Samples = 1 */ |
| #define | ISL29023_CMD_I_PRST_4 ((uint8_t) 0x01) /* Number of Integration Samples = 4 */ |
| #define | ISL29023_CMD_I_PRST_8 ((uint8_t) 0x02) /* Number of Integration Samples = 8 */ |
| #define | ISL29023_CMD_I_PRST_16 ((uint8_t) 0x03) /* Number of Integration Samples = 16 */ |
| #define | ISL29023_CMD_I_FLAG_CLEARED ((uint8_t) 0x00) /* IRQ flag is cleared or not triggered yet */ |
| #define | ISL29023_CMD_I_FLAG_TRIGGERED ((uint8_t) 0x04) /* IRQ flag is triggered */ |
| #define | ISL29023_CMD_I_OP_POWER_DOWN ((uint8_t) 0x00) /* Power-down the device (default) */ |
| #define | ISL29023_CMD_I_OP_ALS_ONCE ((uint8_t) 0x20) /* IC measures ALS only once */ |
| #define | ISL29023_CMD_I_OP_IR_ONCE ((uint8_t) 0x40) /* IC meausres IR only once */ |
| #define | ISL29023_CMD_I_OP_ALS_CONT ((uint8_t) 0xA0) /* IC meausres ALS continuously */ |
| #define | ISL29023_CMD_I_OP_IR_CONT ((uint8_t) 0xC0) /* IC meausres IR continuous */ |
| #define | ISL29023_CMD_II_RANGE_MASK ((uint8_t) 0x03) |
| #define | ISL29023_CMD_II_RANGE_SHIFT ((uint8_t) 0) |
| #define | ISL29023_CMD_II_RES_MASK ((uint8_t) 0x0C) |
| #define | ISL29023_CMD_II_RES_SHIFT ((uint8_t) 2) |
| #define | ISL29023_CMD_II_RANGE_1 ((uint8_t) 0x00) /* FSR @ALS Sensing = 1.000 */ |
| #define | ISL29023_CMD_II_RANGE_2 ((uint8_t) 0x01) /* FSR @ALS Sensing = 4.000 */ |
| #define | ISL29023_CMD_II_RANGE_3 ((uint8_t) 0x02) /* FSR @ALS Sensing = 16.000 */ |
| #define | ISL29023_CMD_II_RANGE_4 ((uint8_t) 0x03) /* FSR @ALS Sensing = 64.000 */ |
| #define | ISL29023_CMD_II_RES_16 ((uint8_t) 0x00) /* 2^16 ADC resolution */ |
| #define | ISL29023_CMD_II_RES_12 ((uint8_t) 0x04) /* 2^12 ADC resolution */ |
| #define | ISL29023_CMD_II_RES_8 ((uint8_t) 0x08) /* 2^8 ADC resolution */ |
| #define | ISL29023_CMD_II_RES_4 ((uint8_t) 0x0C) /* 2^4 ADC resolution */ |
Typedefs | |
| typedef uint8_t | ISL29023_DATA_LSB_t |
| typedef uint8_t | ISL29023_DATA_MSB_t |
| typedef uint8_t | ISL29023_INT_LT_LSB_t |
| typedef uint8_t | ISL29023_INT_LT_MSB_t |
| typedef uint8_t | ISL29023_INT_HT_LSB_t |
| typedef uint8_t | ISL29023_INT_HT_MSB_t |
| typedef uint8_t | ISL29023_TEST_t |
Enumerations | |
| enum | { ISL29023_CMD_I = 0x00, ISL29023_CMD_II = 0x01, ISL29023_DATA_LSB = 0x02, ISL29023_DATA_MSB = 0x03, ISL29023_INT_LT_LSB = 0x04, ISL29023_INT_LT_MSB = 0x05, ISL29023_INT_HT_LSB = 0x06, ISL29023_INT_HT_MSB = 0x07, ISL29023_TEST = 0x08 } |
| #define ISL29023_CMD_I_FLAG_CLEARED ((uint8_t) 0x00) /* IRQ flag is cleared or not triggered yet */ |
Definition at line 69 of file isl29023.h.
| #define ISL29023_CMD_I_FLAG_MASK ((uint8_t) 0x04) |
Definition at line 55 of file isl29023.h.
Referenced by main().
| #define ISL29023_CMD_I_FLAG_SHIFT ((uint8_t) 2) |
Definition at line 56 of file isl29023.h.
| #define ISL29023_CMD_I_FLAG_TRIGGERED ((uint8_t) 0x04) /* IRQ flag is triggered */ |
Definition at line 70 of file isl29023.h.
| #define ISL29023_CMD_I_OP_ALS_CONT ((uint8_t) 0xA0) /* IC meausres ALS continuously */ |
Definition at line 74 of file isl29023.h.
| #define ISL29023_CMD_I_OP_ALS_ONCE ((uint8_t) 0x20) /* IC measures ALS only once */ |
Definition at line 72 of file isl29023.h.
| #define ISL29023_CMD_I_OP_IR_CONT ((uint8_t) 0xC0) /* IC meausres IR continuous */ |
Definition at line 75 of file isl29023.h.
| #define ISL29023_CMD_I_OP_IR_ONCE ((uint8_t) 0x40) /* IC meausres IR only once */ |
Definition at line 73 of file isl29023.h.
| #define ISL29023_CMD_I_OP_MASK ((uint8_t) 0xe0) |
Definition at line 58 of file isl29023.h.
Referenced by ISL29023_I2C_DeInit().
| #define ISL29023_CMD_I_OP_POWER_DOWN ((uint8_t) 0x00) /* Power-down the device (default) */ |
Definition at line 71 of file isl29023.h.
Referenced by ISL29023_I2C_DeInit().
| #define ISL29023_CMD_I_OP_SHIFT ((uint8_t) 5) |
Definition at line 59 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_1 ((uint8_t) 0x00) /* Number of Integration Samples = 1 */ |
Definition at line 65 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_16 ((uint8_t) 0x03) /* Number of Integration Samples = 16 */ |
Definition at line 68 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_4 ((uint8_t) 0x01) /* Number of Integration Samples = 4 */ |
Definition at line 66 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_8 ((uint8_t) 0x02) /* Number of Integration Samples = 8 */ |
Definition at line 67 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_MASK ((uint8_t) 0x03) |
Definition at line 52 of file isl29023.h.
| #define ISL29023_CMD_I_PRST_SHIFT ((uint8_t) 0) |
Definition at line 53 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_1 ((uint8_t) 0x00) /* FSR @ALS Sensing = 1.000 */ |
Definition at line 113 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_2 ((uint8_t) 0x01) /* FSR @ALS Sensing = 4.000 */ |
Definition at line 114 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_3 ((uint8_t) 0x02) /* FSR @ALS Sensing = 16.000 */ |
Definition at line 115 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_4 ((uint8_t) 0x03) /* FSR @ALS Sensing = 64.000 */ |
Definition at line 116 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_MASK ((uint8_t) 0x03) |
Definition at line 103 of file isl29023.h.
| #define ISL29023_CMD_II_RANGE_SHIFT ((uint8_t) 0) |
Definition at line 104 of file isl29023.h.
| #define ISL29023_CMD_II_RES_12 ((uint8_t) 0x04) /* 2^12 ADC resolution */ |
Definition at line 118 of file isl29023.h.
| #define ISL29023_CMD_II_RES_16 ((uint8_t) 0x00) /* 2^16 ADC resolution */ |
Definition at line 117 of file isl29023.h.
| #define ISL29023_CMD_II_RES_4 ((uint8_t) 0x0C) /* 2^4 ADC resolution */ |
Definition at line 120 of file isl29023.h.
| #define ISL29023_CMD_II_RES_8 ((uint8_t) 0x08) /* 2^8 ADC resolution */ |
Definition at line 119 of file isl29023.h.
| #define ISL29023_CMD_II_RES_MASK ((uint8_t) 0x0C) |
Definition at line 106 of file isl29023.h.
| #define ISL29023_CMD_II_RES_SHIFT ((uint8_t) 2) |
Definition at line 107 of file isl29023.h.
| #define ISL29023_I2C_ADDRESS (0x44) /*ISL29023 I2C Address */ |
Definition at line 26 of file isl29023.h.
Referenced by main().
| #define ISL29023_I2C_TEST_VALUE (0x00) /*ISL29023 test register value */ |
Definition at line 27 of file isl29023.h.
Referenced by main().
| typedef uint8_t ISL29023_DATA_LSB_t |
Definition at line 131 of file isl29023.h.
| typedef uint8_t ISL29023_DATA_MSB_t |
Definition at line 140 of file isl29023.h.
| typedef uint8_t ISL29023_INT_HT_LSB_t |
Definition at line 167 of file isl29023.h.
| typedef uint8_t ISL29023_INT_HT_MSB_t |
Definition at line 176 of file isl29023.h.
| typedef uint8_t ISL29023_INT_LT_LSB_t |
Definition at line 149 of file isl29023.h.
| typedef uint8_t ISL29023_INT_LT_MSB_t |
Definition at line 158 of file isl29023.h.
| typedef uint8_t ISL29023_TEST_t |
Definition at line 185 of file isl29023.h.
| anonymous enum |
ISL29023 Ambient Light Sensor Internal Registers
| Enumerator | |
|---|---|
| ISL29023_CMD_I | |
| ISL29023_CMD_II | |
| ISL29023_DATA_LSB | |
| ISL29023_DATA_MSB | |
| ISL29023_INT_LT_LSB | |
| ISL29023_INT_LT_MSB | |
| ISL29023_INT_HT_LSB | |
| ISL29023_INT_HT_MSB | |
| ISL29023_TEST | |
Definition at line 14 of file isl29023.h.