15 #include "Driver_SPI.h"    32     uint8_t cocoBuffer[2] = {0};
    35     if ((pCommDrv == NULL) || (pCommandList == NULL))
    46         if (ARM_DRIVER_OK != status)
    54             status = 
Register_SPI_Read(pCommDrv, devInfo, pWriteParams, 0, 
sizeof(cocoBuffer), cocoBuffer);
    55             if (ARM_DRIVER_OK != status)
    59             commandComplete = cocoBuffer[1] & 0x80;
    60             if (commandComplete && cocoBuffer[1] & error_mask)
    64         } 
while (!commandComplete);
    65     } 
while ((++pCmd)->writeTo != 0xFFFF);
    77     bool endDataMarkAwaited;
    80     if ((pCommDrv == NULL) || (pRegWriteList == NULL))
    90         endDataMarkAwaited = (pCmd + 1)->writeTo != 0xFFFF;
    93         if (ARM_DRIVER_OK != status)
    98     } 
while (endDataMarkAwaited);
   114     if (pCommDrv == NULL || pReadList == NULL || pOutBuffer == NULL)
   122     for (pBuf = pOutBuffer; pCmd->
numBytes != 0; pCmd++)
   125         if (ARM_DRIVER_OK != status)
 
This structure defines the device specific info required by register I/O. 
 
This structure defines the Write command List. 
 
The sensor_io_spi.h file declares low-level interface functions for reading and writing sensor regist...
 
void BOARD_DELAY_ms(uint32_t delay_ms)
Function to insert delays. 
 
This structure defines the Block command List. 
 
int32_t Register_SPI_Write(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, uint8_t offset, uint8_t value, uint8_t mask)
The interface function to write a sensor register. 
 
The sensor_drv.h file contains sensor state and error definitions. 
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
int32_t Sensor_SPI_Read(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pReadParams, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor. 
 
int32_t Sensor_SPI_BlockWrite(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, const registercommandlist_t *pCommandList, uint8_t error_mask)
Write commands to a sensor. 
 
int32_t Register_SPI_BlockWrite(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, uint8_t offset, const uint8_t *pBuffer, uint8_t bytesToWrite)
The interface function to block write to a sensor register. 
 
This structure defines the Read command List. 
 
int32_t Sensor_SPI_Write(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, const registerwritelist_t *pRegWriteList)
Write register data to a sensor. 
 
const uint8_t * pWriteBuffer
 
int32_t Register_SPI_Read(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pReadParams, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register.