ISSDK  1.8
IoT Sensing Software Development Kit
Functions
systick_utils.h File Reference

ARM Systick Utilities. More...

Go to the source code of this file.

Functions

void BOARD_SystickEnable (void)
 Function to enable systicks framework. More...
 
void BOARD_SystickStart (int32_t *pStart)
 Function to Record the Start systick. More...
 
int32_t BOARD_SystickElapsedTicks (int32_t *pStart)
 Function to compute the Elapsed systicks. More...
 
uint32_t BOARD_SystickElapsedTime_us (int32_t *pStart)
 Function to compute the Elapsed Time. More...
 
void BOARD_DELAY_ms (uint32_t delay_ms)
 Function to insert delays. More...
 

Detailed Description

ARM Systick Utilities.

This file provides systick based counts for the developer to get cycle counts for measuring time delays.

Definition in file systick_utils.h.

Function Documentation

◆ BOARD_DELAY_ms()

void BOARD_DELAY_ms ( uint32_t  delay_ms)

Function to insert delays.

This function blocks for the specified milli seconds by using the elapsed systicks to determine time delays.

Parameters
[in]delay_msThe required time to block.
Returns
void.
Constraints:
None. Yes

Definition at line 81 of file systick_utils.c.

References BOARD_SystickElapsedTicks(), BOARD_SystickStart(), and int32_t().

Referenced by ADS_DetectShield(), ADS_MMA9553Query(), FXLC95000_SPI_Initialize(), FXLS8962_I2C_DeInit(), FXLS8962_SPI_Deinit(), FXLS896x_I2C_DeInit(), FXLS896x_SPI_Deinit(), FXLS8974_I2C_DeInit(), FXLS8974_SPI_Deinit(), MMA9553_I2C_Initialize(), MMA9553_SPI_Initialize(), perform_selftest(), Sensor_I2C_BlockWrite(), and Sensor_SPI_BlockWrite().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ BOARD_SystickElapsedTicks()

int32_t BOARD_SystickElapsedTicks ( int32_t *  pStart)

Function to compute the Elapsed systicks.

This function computes the elapsed ticks by getting the difference of the current tick to the one in the arguement.

Parameters
[in]pStartPointer to the variable contating the start systick.
Returns
int32_t The elapsed systicks.
Constraints:
None. Yes

Definition at line 52 of file systick_utils.c.

References g_ovf_counter, g_ovf_stamp, int32_t(), SYST_CVR, and SYST_RVR.

Referenced by BOARD_DELAY_ms(), and BOARD_SystickElapsedTime_us().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ BOARD_SystickElapsedTime_us()

uint32_t BOARD_SystickElapsedTime_us ( int32_t *  pStart)

Function to compute the Elapsed Time.

This function computes the elapsed Time in micro seconds by getting the difference of the current tick to the one in the arguement. It also updates the start tick to the current systick.

Parameters
[in]pStartPointer to the variable contating the start systick.
Returns
uint32_t The elapsed Time in micro seconds.
Constraints:
None. Yes

Definition at line 64 of file systick_utils.c.

References BOARD_SystickElapsedTicks(), and BOARD_SystickStart().

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ BOARD_SystickEnable()

void BOARD_SystickEnable ( void  )

Function to enable systicks framework.

This function initializes the CMSIS define ARM core specific systick implementation.

Parameters
[in]void.
Returns
void.
Constraints:
This should be the first function to be invoked before other Systick APIs. Yes

Definition at line 35 of file systick_utils.c.

References SYST_CSR, and SYST_RVR.

Referenced by main().

Here is the caller graph for this function:

◆ BOARD_SystickStart()

void BOARD_SystickStart ( int32_t *  pStart)

Function to Record the Start systick.

This function records the current systick count for other APIs to compute difference.

Parameters
[in]pStartPointer to the variable to store the current/start systick.
Returns
void.
Constraints:
None. Yes

Definition at line 44 of file systick_utils.c.

References g_ovf_counter, g_ovf_stamp, and SYST_CVR.

Referenced by BOARD_DELAY_ms(), BOARD_SystickElapsedTime_us(), main(), and process_host_command().

Here is the caller graph for this function: