![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The frdm_k64f.c file defines GPIO pins and I2C CMSIS utilities for FRDM-K64F board. More...
#include "frdm_k64f.h"
Go to the source code of this file.
Functions | |
| uint32_t | UART0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART3_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART4_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART5_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | DSPI0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | DSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | DSPI2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The frdm_k64f.c file defines GPIO pins and I2C CMSIS utilities for FRDM-K64F board.
Definition in file frdm_k64f.c.
| uint32_t DSPI0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 334 of file frdm_k64f.c.
| uint32_t DSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 346 of file frdm_k64f.c.
| uint32_t DSPI2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 358 of file frdm_k64f.c.
| uint32_t I2C0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 298 of file frdm_k64f.c.
| uint32_t I2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 310 of file frdm_k64f.c.
| uint32_t I2C2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 322 of file frdm_k64f.c.
| uint32_t UART0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 226 of file frdm_k64f.c.
| uint32_t UART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 238 of file frdm_k64f.c.
| uint32_t UART2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 250 of file frdm_k64f.c.
| uint32_t UART3_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 262 of file frdm_k64f.c.
| uint32_t UART4_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 274 of file frdm_k64f.c.
| uint32_t UART5_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 286 of file frdm_k64f.c.
Definition at line 88 of file frdm_k64f.c.
Definition at line 95 of file frdm_k64f.c.
Definition at line 102 of file frdm_k64f.c.
Definition at line 109 of file frdm_k64f.c.
Definition at line 40 of file frdm_k64f.c.
Definition at line 33 of file frdm_k64f.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 195 of file frdm_k64f.c.
Definition at line 72 of file frdm_k64f.c.
Definition at line 79 of file frdm_k64f.c.
| gpioHandleKSDK_t D10 |
Definition at line 172 of file frdm_k64f.c.
| gpioHandleKSDK_t D11 |
Definition at line 56 of file frdm_k64f.c.
| gpioHandleKSDK_t D12 |
Definition at line 63 of file frdm_k64f.c.
| gpioHandleKSDK_t D13 |
Definition at line 49 of file frdm_k64f.c.
| gpioHandleKSDK_t D14 |
Definition at line 24 of file frdm_k64f.c.
| gpioHandleKSDK_t D15 |
Definition at line 17 of file frdm_k64f.c.
Definition at line 116 of file frdm_k64f.c.
Definition at line 123 of file frdm_k64f.c.
Definition at line 130 of file frdm_k64f.c.
Definition at line 137 of file frdm_k64f.c.
Definition at line 144 of file frdm_k64f.c.
Definition at line 151 of file frdm_k64f.c.
Definition at line 158 of file frdm_k64f.c.
Definition at line 165 of file frdm_k64f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 188 of file frdm_k64f.c.
Referenced by fxlc95000_enSensor(), initializeStatusSubsystem(), main(), and process_host_command().
| gpioHandleKSDK_t INT1 |
Definition at line 204 of file frdm_k64f.c.
| gpioHandleKSDK_t INT2 |
Definition at line 211 of file frdm_k64f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 181 of file frdm_k64f.c.
Referenced by fxlc95000_enSensor(), initializeStatusSubsystem(), main(), and process_host_command().