22                         .clockName = kCLOCK_PortE,
    29                         .clockName = kCLOCK_PortE,
    38                        .clockName = kCLOCK_PortC,
    45                        .clockName = kCLOCK_PortC,
    54                         .clockName = kCLOCK_PortD,
    61                         .clockName = kCLOCK_PortD,
    68                         .clockName = kCLOCK_PortD,
    77                        .clockName = kCLOCK_PortC,
    84                        .clockName = kCLOCK_PortC,
    93                        .clockName = kCLOCK_PortB,
   100                        .clockName = kCLOCK_PortB,
   107                        .clockName = kCLOCK_PortB,
   114                        .clockName = kCLOCK_PortB,
   121                        .clockName = kCLOCK_PortB,
   128                        .clockName = kCLOCK_PortA,
   135                        .clockName = kCLOCK_PortB,
   142                        .clockName = kCLOCK_PortA,
   149                        .clockName = kCLOCK_PortC,
   156                        .clockName = kCLOCK_PortC,
   163                        .clockName = kCLOCK_PortA,
   170                        .clockName = kCLOCK_PortC,
   177                         .clockName = kCLOCK_PortD,
   186                             .clockName = kCLOCK_PortB,
   193                               .clockName = kCLOCK_PortE,
   200                              .clockName = kCLOCK_PortB,
   209                          .clockName = kCLOCK_PortC,
   216                          .clockName = kCLOCK_PortC,
   228     return CLOCK_GetFreq(UART0_CLK_SRC);
   240     return CLOCK_GetFreq(UART1_CLK_SRC);
   252     return CLOCK_GetFreq(UART2_CLK_SRC);
   264     return CLOCK_GetFreq(UART3_CLK_SRC);
   276     return CLOCK_GetFreq(UART4_CLK_SRC);
   288     return CLOCK_GetFreq(UART5_CLK_SRC);
   300     return CLOCK_GetFreq(I2C0_CLK_SRC);
   312     return CLOCK_GetFreq(I2C1_CLK_SRC);
   324     return CLOCK_GetFreq(I2C2_CLK_SRC);
   336     return CLOCK_GetBusClkFreq();
   348     return CLOCK_GetBusClkFreq();
   360     return CLOCK_GetBusClkFreq();
 
uint32_t DSPI2_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART4_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART3_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t I2C2_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t I2C1_GetFreq(void)
Determines the Clock Frequency feature. 
 
The GPIO pin handle for KSDK. 
 
uint32_t DSPI0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART5_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t DSPI1_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART1_GetFreq(void)
Determines the Clock Frequency feature. 
 
The frdm_k64f.h file defines GPIO pin mappings for FRDM-K64F board. 
 
uint32_t I2C0_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t BLUE_LED
 
uint32_t UART2_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t GREEN_LED