![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The frdm_kl25z.c file defines GPIO pins for FRDM-KL25Z board. More...
#include "frdm_kl25z.h"
Go to the source code of this file.
Functions | |
| uint32_t | UART0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | SPI0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | SPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The frdm_kl25z.c file defines GPIO pins for FRDM-KL25Z board.
Definition in file frdm_kl25z.c.
| uint32_t I2C0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 271 of file frdm_kl25z.c.
| uint32_t I2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 283 of file frdm_kl25z.c.
| uint32_t SPI0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 295 of file frdm_kl25z.c.
| uint32_t SPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 307 of file frdm_kl25z.c.
| uint32_t UART0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 234 of file frdm_kl25z.c.
| uint32_t UART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 247 of file frdm_kl25z.c.
| uint32_t UART2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 259 of file frdm_kl25z.c.
Definition at line 88 of file frdm_kl25z.c.
Definition at line 95 of file frdm_kl25z.c.
Definition at line 102 of file frdm_kl25z.c.
Definition at line 40 of file frdm_kl25z.c.
Definition at line 33 of file frdm_kl25z.c.
| gpioHandleKSDK_t ACCEL_SCL |
Definition at line 197 of file frdm_kl25z.c.
| gpioHandleKSDK_t ACCEL_SDA |
Definition at line 204 of file frdm_kl25z.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 188 of file frdm_kl25z.c.
Definition at line 72 of file frdm_kl25z.c.
Definition at line 79 of file frdm_kl25z.c.
| gpioHandleKSDK_t D10 |
Definition at line 165 of file frdm_kl25z.c.
| gpioHandleKSDK_t D11 |
Definition at line 56 of file frdm_kl25z.c.
| gpioHandleKSDK_t D12 |
Definition at line 63 of file frdm_kl25z.c.
| gpioHandleKSDK_t D13 |
Definition at line 49 of file frdm_kl25z.c.
| gpioHandleKSDK_t D14 |
Definition at line 24 of file frdm_kl25z.c.
| gpioHandleKSDK_t D15 |
Definition at line 17 of file frdm_kl25z.c.
Definition at line 109 of file frdm_kl25z.c.
Definition at line 116 of file frdm_kl25z.c.
Definition at line 123 of file frdm_kl25z.c.
Definition at line 130 of file frdm_kl25z.c.
Definition at line 137 of file frdm_kl25z.c.
Definition at line 144 of file frdm_kl25z.c.
Definition at line 151 of file frdm_kl25z.c.
Definition at line 158 of file frdm_kl25z.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 181 of file frdm_kl25z.c.
| gpioHandleKSDK_t INT1 |
Definition at line 212 of file frdm_kl25z.c.
| gpioHandleKSDK_t INT2 |
Definition at line 219 of file frdm_kl25z.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 174 of file frdm_kl25z.c.