22                         .clockName = kCLOCK_PortE,
    29                         .clockName = kCLOCK_PortE,
    38                        .clockName = kCLOCK_PortC,
    45                        .clockName = kCLOCK_PortC,
    54                         .clockName = kCLOCK_PortD,
    61                         .clockName = kCLOCK_PortD,
    68                         .clockName = kCLOCK_PortD,
    77                        .clockName = kCLOCK_PortA,
    84                        .clockName = kCLOCK_PortA,
    93                        .clockName = kCLOCK_PortB,
   100                        .clockName = kCLOCK_PortB,
   106                        .irq = NotAvail_IRQn,
   107                        .clockName = kCLOCK_PortB,
   114                        .clockName = kCLOCK_PortD,
   121                        .clockName = kCLOCK_PortA,
   128                        .clockName = kCLOCK_PortA,
   135                        .clockName = kCLOCK_PortA,
   141                        .irq = NotAvail_IRQn,
   142                        .clockName = kCLOCK_PortC,
   148                        .irq = NotAvail_IRQn,
   149                        .clockName = kCLOCK_PortC,
   156                        .clockName = kCLOCK_PortA,
   163                        .clockName = kCLOCK_PortD,
   170                         .clockName = kCLOCK_PortD,
   178                             .irq = NotAvail_IRQn,
   179                             .clockName = kCLOCK_PortB,
   185                               .irq = NotAvail_IRQn,
   186                               .clockName = kCLOCK_PortB,
   193                              .clockName = kCLOCK_PortD,
   201                               .irq = NotAvail_IRQn,
   202                               .clockName = kCLOCK_PortE,
   208                               .irq = NotAvail_IRQn,
   209                               .clockName = kCLOCK_PortE,
   217                          .clockName = kCLOCK_PortA,
   224                          .clockName = kCLOCK_PortA,
   236     CLOCK_SetLpsci0Clock(1);
   237     return CLOCK_GetFreq(kCLOCK_CoreSysClk);
   249     return CLOCK_GetFreq(UART1_CLK_SRC);
   261     return CLOCK_GetFreq(UART2_CLK_SRC);
   273     return CLOCK_GetFreq(I2C0_CLK_SRC);
   285     return CLOCK_GetFreq(I2C1_CLK_SRC);
   297     return CLOCK_GetBusClkFreq();
   309     return CLOCK_GetBusClkFreq();
 gpioHandleKSDK_t BLUE_LED
 
gpioHandleKSDK_t ACCEL_SDA
 
uint32_t I2C1_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t SPI1_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART2_GetFreq(void)
Determines the Clock Frequency feature. 
 
The GPIO pin handle for KSDK. 
 
gpioHandleKSDK_t GREEN_LED
 
uint32_t UART0_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t ACCEL_SCL
 
The frdm_kl25z.h file defines GPIO pin mappings for FRDM-KL25Z board. 
 
uint32_t I2C0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t SPI0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t UART1_GetFreq(void)
Determines the Clock Frequency feature.