20                         .clockName = kCLOCK_Gpio0,
    21                         .portNumber = kGINT_Port0};
    25                         .clockName = kCLOCK_Gpio0,
    26                         .portNumber = kGINT_Port0};
    32                         .clockName = kCLOCK_Gpio0,
    33                         .portNumber = kGINT_Port0};
    37                         .clockName = kCLOCK_Gpio0,
    38                         .portNumber = kGINT_Port0};
    42                         .clockName = kCLOCK_Gpio0,
    43                         .portNumber = kGINT_Port0};
    49                        .clockName = kCLOCK_Gpio0,
    50                        .portNumber = kGINT_Port0};
    54                        .clockName = kCLOCK_Gpio0,
    55                        .portNumber = kGINT_Port0};
    61                        .clockName = kCLOCK_Gpio0,
    62                        .portNumber = kGINT_Port0};
    67                        .clockName = kCLOCK_Gpio1,
    68                        .portNumber = kGINT_Port1};
    72                        .clockName = kCLOCK_Gpio1,
    73                        .portNumber = kGINT_Port1};
    77                        .clockName = kCLOCK_Gpio1,
    78                        .portNumber = kGINT_Port1};
    82                        .clockName = kCLOCK_Gpio1,
    83                        .portNumber = kGINT_Port1};
    88                        .clockName = kCLOCK_Gpio0,
    89                        .portNumber = kGINT_Port0};
    93                        .clockName = kCLOCK_Gpio1,
    94                        .portNumber = kGINT_Port1};
    98                        .clockName = kCLOCK_Gpio1,
    99                        .portNumber = kGINT_Port1};
   103                        .clockName = kCLOCK_Gpio0,
   104                        .portNumber = kGINT_Port0};
   108                        .clockName = kCLOCK_Gpio1,
   109                        .portNumber = kGINT_Port1};
   113                        .clockName = kCLOCK_Gpio1,
   114                        .portNumber = kGINT_Port1};
   118                        .clockName = kCLOCK_Gpio1,
   119                        .portNumber = kGINT_Port1};
   123                        .clockName = kCLOCK_Gpio1,
   124                        .portNumber = kGINT_Port1};
   128                         .clockName = kCLOCK_Gpio1,
   129                         .portNumber = kGINT_Port1};
   135                             .clockName = kCLOCK_Gpio0,
   136                             .portNumber = kGINT_Port0};
   140                               .clockName = kCLOCK_Gpio1,
   141                               .portNumber = kGINT_Port1};
   145                              .clockName = kCLOCK_Gpio1,
   146                              .portNumber = kGINT_Port1};
   159     return kStatus_Success;
   173     return kStatus_Success;
   185     return CLOCK_GetFreq(kCLOCK_Flexcomm0);
   197     return CLOCK_GetFreq(kCLOCK_Fro12M);
   209     return CLOCK_GetFreq(kCLOCK_Fro12M);
   221     return CLOCK_GetFreq(kCLOCK_Flexcomm3);
   233     return CLOCK_GetFreq(kCLOCK_Flexcomm5);
 
uint32_t SPI3_GetFreq(void)
Determines the Clock Frequency feature. 
 
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
 
uint32_t I2C5_GetFreq(void)
Determines the Clock Frequency feature. 
 
The GPIO pin handle for KSDK. 
 
The lpc54114.h file defines GPIO pin mappings for LPCXpresso54114 board. 
 
uint32_t USART0_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t BLUE_LED
 
uint32_t SPI5_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t GREEN_LED
 
uint32_t I2C4_GetFreq(void)
Determines the Clock Frequency feature. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...