![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mekmimx8qm.h file defines GPIO pin mappings and on-board sensors information for mekmimx8qm board. More...
#include "pin_mux.h"#include "RTE_Device.h"#include "gpio_driver.h"#include "main/imx8qm_pads.h"#include "svc/pad/pad_api.h"

Go to the source code of this file.
Macros | |
| #define | I2C_BB_SCL_PIN SC_P_HDMI_TX0_TS_SCL |
| #define | I2C_BB_SDA_PIN SC_P_HDMI_TX0_TS_SDA |
| #define | I2C_BB_DRIVER Driver_I2C2 |
| #define | I2C_BB_DEVICE_INDEX I2C2_INDEX |
| #define | I2C_BB_SIGNAL_EVENT I2C2_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART0 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | FXOS8700_BB_I2C_ADDR 0x1E |
| #define | FXAS21002_BB_I2C_ADDR 0x20 |
| #define | MPL3115_BB_I2C_ADDR 0x60 |
| #define | ASK_USER_TO_RESUME(x) |
| #define | I2C2 LPI2C2 |
| #define | I2C_Type LPI2C_Type |
| #define | I2C_BASE_PTRS LPI2C_BASE_PTRS |
| #define | SPI1 LPSPI1 |
| #define | SPI_Type LPSPI_Type |
| #define | SPI_BASE_PTRS LPSPI_BASE_PTRS |
| #define | FXAS21002_I2C_ADDR FXAS21002_BB_I2C_ADDR |
| #define | FXOS8700_I2C_ADDR FXOS8700_BB_I2C_ADDR |
| #define | MPL3115_I2C_ADDR MPL3115_BB_I2C_ADDR |
| #define | SMC NULL |
Functions | |
| status_t | SMC_SetPowerModeWait (void *) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
The mekmimx8qm.h file defines GPIO pin mappings and on-board sensors information for mekmimx8qm board.
Definition in file mekmimx8qm.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 49 of file mekmimx8qm.h.
| #define FXAS21002_BB_I2C_ADDR 0x20 |
Definition at line 39 of file mekmimx8qm.h.
| #define FXAS21002_I2C_ADDR FXAS21002_BB_I2C_ADDR |
Definition at line 68 of file mekmimx8qm.h.
| #define FXOS8700_BB_I2C_ADDR 0x1E |
Definition at line 34 of file mekmimx8qm.h.
| #define FXOS8700_I2C_ADDR FXOS8700_BB_I2C_ADDR |
Definition at line 69 of file mekmimx8qm.h.
| #define HOST_S_DRIVER Driver_USART0 |
Definition at line 30 of file mekmimx8qm.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 31 of file mekmimx8qm.h.
| #define I2C2 LPI2C2 |
Definition at line 60 of file mekmimx8qm.h.
| #define I2C_BASE_PTRS LPI2C_BASE_PTRS |
Definition at line 62 of file mekmimx8qm.h.
| #define I2C_BB_DEVICE_INDEX I2C2_INDEX |
Definition at line 26 of file mekmimx8qm.h.
| #define I2C_BB_DRIVER Driver_I2C2 |
Definition at line 25 of file mekmimx8qm.h.
| #define I2C_BB_SCL_PIN SC_P_HDMI_TX0_TS_SCL |
Definition at line 23 of file mekmimx8qm.h.
| #define I2C_BB_SDA_PIN SC_P_HDMI_TX0_TS_SDA |
Definition at line 24 of file mekmimx8qm.h.
| #define I2C_BB_SIGNAL_EVENT I2C2_SignalEvent_t |
Definition at line 27 of file mekmimx8qm.h.
| #define I2C_Type LPI2C_Type |
Definition at line 61 of file mekmimx8qm.h.
| #define MPL3115_BB_I2C_ADDR 0x60 |
Definition at line 44 of file mekmimx8qm.h.
| #define MPL3115_I2C_ADDR MPL3115_BB_I2C_ADDR |
Definition at line 70 of file mekmimx8qm.h.
| #define SMC NULL |
Definition at line 73 of file mekmimx8qm.h.
| #define SPI1 LPSPI1 |
Definition at line 63 of file mekmimx8qm.h.
| #define SPI_BASE_PTRS LPSPI_BASE_PTRS |
Definition at line 65 of file mekmimx8qm.h.
| #define SPI_Type LPSPI_Type |
Definition at line 64 of file mekmimx8qm.h.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 169 of file lpc54114.c.
Referenced by BOARD_BootClockVLPR(), fxlc95000_enSensor(), and main().

| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 155 of file lpc54114.c.
Referenced by main().