![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
#include "pin_mux.h"#include "fsl_msmc.h"#include "RTE_Device.h"#include "gpio_driver.h"#include "K32W042S1M2_cm4.h"

Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN D15 |
| #define | I2C_S1_SDA_PIN D14 |
| #define | I2C_S1_DRIVER Driver_I2C0 |
| #define | I2C_S1_DEVICE_INDEX I2C0_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
| #define | I2C_S2_SCL_PIN A5 |
| #define | I2C_S2_SDA_PIN A4 |
| #define | I2C_S2_DRIVER Driver_I2C3 |
| #define | I2C_S2_DEVICE_INDEX I2C3_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C3_SignalEvent_t |
| #define | I2C_BB_SCL_PIN A5 |
| #define | I2C_BB_SDA_PIN A4 |
| #define | I2C_BB_DRIVER Driver_I2C3 |
| #define | I2C_BB_DEVICE_INDEX I2C3_INDEX |
| #define | I2C_BB_SIGNAL_EVENT I2C3_SignalEvent_t |
| #define | SPI_S_SCLK D13 |
| #define | SPI_S_MISO D12 |
| #define | SPI_S_MOSI D11 |
| #define | SPI_S_DRIVER Driver_SPI0 |
| #define | SPI_S_BAUDRATE 500000U |
| Transfer baudrate - 500k. More... | |
| #define | SPI_S_DEVICE_INDEX SPI0_INDEX |
| #define | SPI_S_SIGNAL_EVENT SPI0_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART0 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | HOST_B_DRIVER Driver_USART1 |
| #define | HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | FXOS8700_BB_I2C_ADDR 0x1E |
| #define | FXOS8700_BB_INT1 INT1 |
| #define | FXOS8700_BB_INT2 INT2 |
| #define | ASK_USER_TO_RESUME(x) |
| #define | ADS_NVM_ADDR 0x000BF000 |
| start of the next to last 4K (sector size) of the 768K flash More... | |
| #define | FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
| #define | SMC SMC0 |
| #define | I2C0 LPI2C0 |
| #define | I2C3 LPI2C3 |
| #define | I2C_Type LPI2C_Type |
| #define | I2C_BASE_PTRS LPI2C_BASE_PTRS |
| #define | SPI0 LPSPI0 |
| #define | SPI_Type LPSPI_Type |
| #define | SPI_BASE_PTRS LPSPI_BASE_PTRS |
| #define ADS_NVM_ADDR 0x000BF000 |
start of the next to last 4K (sector size) of the 768K flash
Definition at line 116 of file frdm_k32l3a6.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 105 of file frdm_k32l3a6.h.
| #define FLASH_SECTOR_SIZE_PROPERTY kFLASH_PropertyPflashSectorSize |
Definition at line 117 of file frdm_k32l3a6.h.
| #define FXOS8700_BB_I2C_ADDR 0x1E |
Definition at line 100 of file frdm_k32l3a6.h.
| #define FXOS8700_BB_INT1 INT1 |
Definition at line 101 of file frdm_k32l3a6.h.
| #define FXOS8700_BB_INT2 INT2 |
Definition at line 102 of file frdm_k32l3a6.h.
| #define HOST_B_DRIVER Driver_USART1 |
Definition at line 96 of file frdm_k32l3a6.h.
| #define HOST_B_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 97 of file frdm_k32l3a6.h.
| #define HOST_S_DRIVER Driver_USART0 |
Definition at line 92 of file frdm_k32l3a6.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 93 of file frdm_k32l3a6.h.
| #define I2C0 LPI2C0 |
Definition at line 121 of file frdm_k32l3a6.h.
| #define I2C3 LPI2C3 |
Definition at line 122 of file frdm_k32l3a6.h.
| #define I2C_BASE_PTRS LPI2C_BASE_PTRS |
Definition at line 124 of file frdm_k32l3a6.h.
| #define I2C_BB_DEVICE_INDEX I2C3_INDEX |
Definition at line 79 of file frdm_k32l3a6.h.
| #define I2C_BB_DRIVER Driver_I2C3 |
Definition at line 78 of file frdm_k32l3a6.h.
| #define I2C_BB_SCL_PIN A5 |
Definition at line 76 of file frdm_k32l3a6.h.
| #define I2C_BB_SDA_PIN A4 |
Definition at line 77 of file frdm_k32l3a6.h.
| #define I2C_BB_SIGNAL_EVENT I2C3_SignalEvent_t |
Definition at line 80 of file frdm_k32l3a6.h.
| #define I2C_S1_DEVICE_INDEX I2C0_INDEX |
Definition at line 65 of file frdm_k32l3a6.h.
| #define I2C_S1_DRIVER Driver_I2C0 |
Definition at line 64 of file frdm_k32l3a6.h.
| #define I2C_S1_SCL_PIN D15 |
Definition at line 62 of file frdm_k32l3a6.h.
| #define I2C_S1_SDA_PIN D14 |
Definition at line 63 of file frdm_k32l3a6.h.
| #define I2C_S1_SIGNAL_EVENT I2C0_SignalEvent_t |
Definition at line 66 of file frdm_k32l3a6.h.
| #define I2C_S2_DEVICE_INDEX I2C3_INDEX |
Definition at line 72 of file frdm_k32l3a6.h.
| #define I2C_S2_DRIVER Driver_I2C3 |
Definition at line 71 of file frdm_k32l3a6.h.
| #define I2C_S2_SCL_PIN A5 |
Definition at line 69 of file frdm_k32l3a6.h.
| #define I2C_S2_SDA_PIN A4 |
Definition at line 70 of file frdm_k32l3a6.h.
| #define I2C_S2_SIGNAL_EVENT I2C3_SignalEvent_t |
Definition at line 73 of file frdm_k32l3a6.h.
| #define I2C_Type LPI2C_Type |
Definition at line 123 of file frdm_k32l3a6.h.
| #define SMC SMC0 |
Definition at line 120 of file frdm_k32l3a6.h.
| #define SPI0 LPSPI0 |
Definition at line 125 of file frdm_k32l3a6.h.
| #define SPI_BASE_PTRS LPSPI_BASE_PTRS |
Definition at line 127 of file frdm_k32l3a6.h.
| #define SPI_S_BAUDRATE 500000U |
Transfer baudrate - 500k.
Definition at line 87 of file frdm_k32l3a6.h.
| #define SPI_S_DEVICE_INDEX SPI0_INDEX |
Definition at line 88 of file frdm_k32l3a6.h.
| #define SPI_S_DRIVER Driver_SPI0 |
Definition at line 86 of file frdm_k32l3a6.h.
| #define SPI_S_MISO D12 |
Definition at line 84 of file frdm_k32l3a6.h.
| #define SPI_S_MOSI D11 |
Definition at line 85 of file frdm_k32l3a6.h.
| #define SPI_S_SCLK D13 |
Definition at line 83 of file frdm_k32l3a6.h.
| #define SPI_S_SIGNAL_EVENT SPI0_SignalEvent_t |
Definition at line 89 of file frdm_k32l3a6.h.
| #define SPI_Type LPSPI_Type |
Definition at line 126 of file frdm_k32l3a6.h.
Definition at line 88 of file frdm_k64f.c.
Definition at line 95 of file frdm_k64f.c.
Definition at line 102 of file frdm_k64f.c.
Definition at line 109 of file frdm_k64f.c.
Definition at line 40 of file frdm_k64f.c.
Definition at line 33 of file frdm_k64f.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 195 of file frdm_k64f.c.
Definition at line 72 of file frdm_k64f.c.
Definition at line 79 of file frdm_k64f.c.
| gpioHandleKSDK_t D10 |
Definition at line 172 of file frdm_k64f.c.
| gpioHandleKSDK_t D11 |
Definition at line 56 of file frdm_k64f.c.
| gpioHandleKSDK_t D12 |
Definition at line 63 of file frdm_k64f.c.
| gpioHandleKSDK_t D13 |
Definition at line 49 of file frdm_k64f.c.
| gpioHandleKSDK_t D14 |
Definition at line 24 of file frdm_k64f.c.
| gpioHandleKSDK_t D15 |
Definition at line 17 of file frdm_k64f.c.
Definition at line 116 of file frdm_k64f.c.
Definition at line 123 of file frdm_k64f.c.
Definition at line 130 of file frdm_k64f.c.
Definition at line 137 of file frdm_k64f.c.
Definition at line 49 of file frdm_k32l3a6.h.
Definition at line 158 of file frdm_k64f.c.
Definition at line 165 of file frdm_k64f.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 188 of file frdm_k64f.c.
| gpioHandleKSDK_t INT1 |
Definition at line 204 of file frdm_k64f.c.
| gpioHandleKSDK_t INT2 |
Definition at line 211 of file frdm_k64f.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 181 of file frdm_k64f.c.