ISSDK  1.8
IoT Sensing Software Development Kit
Functions
calibration_storage.c File Reference

Provides functions to store calibration to NVM. More...

#include <stdio.h>
#include "sensor_fusion.h"
#include "driver_KSDK_NVM.h"
#include "calibration_storage.h"
Include dependency graph for calibration_storage.c:

Go to the source code of this file.

Functions

void SaveMagCalibrationToNVM (SensorFusionGlobals *sfg)
 
void SaveGyroCalibrationToNVM (SensorFusionGlobals *sfg)
 
void SaveAccelCalibrationToNVM (SensorFusionGlobals *sfg)
 
void EraseMagCalibrationFromNVM (void)
 
void EraseGyroCalibrationFromNVM (void)
 
void EraseAccelCalibrationFromNVM (void)
 

Detailed Description

Provides functions to store calibration to NVM.

Users who are not using NXP hardware will need to supply their own drivers in place of those defined here.

Definition in file calibration_storage.c.

Function Documentation

◆ EraseAccelCalibrationFromNVM()

void EraseAccelCalibrationFromNVM ( void  )

Definition at line 170 of file calibration_storage.c.

References ACCEL_NVM_OFFSET, CALIBRATION_NVM_ADDR, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ EraseGyroCalibrationFromNVM()

void EraseGyroCalibrationFromNVM ( void  )

Definition at line 149 of file calibration_storage.c.

References CALIBRATION_NVM_ADDR, GYRO_NVM_OFFSET, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ EraseMagCalibrationFromNVM()

void EraseMagCalibrationFromNVM ( void  )

Definition at line 128 of file calibration_storage.c.

References CALIBRATION_NVM_ADDR, MAG_NVM_OFFSET, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ SaveAccelCalibrationToNVM()

void SaveAccelCalibrationToNVM ( SensorFusionGlobals *  sfg)

Definition at line 94 of file calibration_storage.c.

References ACCEL_NVM_OFFSET, CALIBRATION_NVM_ADDR, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ SaveGyroCalibrationToNVM()

void SaveGyroCalibrationToNVM ( SensorFusionGlobals *  sfg)

Definition at line 55 of file calibration_storage.c.

References CALIBRATION_NVM_ADDR, F_6DOF_GY_KALMAN, GYRO_NVM_OFFSET, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ SaveMagCalibrationToNVM()

void SaveMagCalibrationToNVM ( SensorFusionGlobals *  sfg)

Definition at line 21 of file calibration_storage.c.

References CALIBRATION_NVM_ADDR, MAG_NVM_OFFSET, SensorFusionGlobals::MagCal, and NVM_SetBlockFlash().

Referenced by DecodeCommandBytes().

Here is the call graph for this function:
Here is the caller graph for this function: