15 #ifndef CPU_LPC54114J256BD64_cm4    16 #include "fsl_flash.h"    18 #include "fsl_flashiap.h"    23 #ifndef CPU_LPC54114J256BD64_cm4    28     uint32_t pflashSectorSize = 
ERROR;
    29     flash_config_t flashDriver;                                            
    32     memset(&flashDriver, 0, 
sizeof(flash_config_t));
    34     result = FLASH_Init(&flashDriver);
    35     if (kStatus_FLASH_Success == result)
    38         result = FLASH_Erase(&flashDriver, Dest, pflashSectorSize,  
FLASH_ERASE_KEY);
    40         if (kStatus_FLASH_Success == result) {
    41             result = FLASH_Program(&flashDriver, Dest, Source, Count);
    42             if (kStatus_FLASH_Success == result)  retVal=
SUCCESS;
    48 byte checkIAPStatus(status_t result) {
    51       case kStatus_FLASHIAP_Success:
    54       case kStatus_FLASHIAP_InvalidCommand :
    57       case kStatus_FLASHIAP_SrcAddrError :
    60       case kStatus_FLASHIAP_DstAddrError :
    63       case kStatus_FLASHIAP_SrcAddrNotMapped :
    66       case kStatus_FLASHIAP_DstAddrNotMapped :
    69       case kStatus_FLASHIAP_CountError :
    72       case kStatus_FLASHIAP_InvalidSector :
    75       case kStatus_FLASHIAP_NotPrepared :
    78       case kStatus_FLASHIAP_CompareError :
    81       case kStatus_FLASHIAP_Busy :
    84       case kStatus_FLASHIAP_ParamError :
    87       case kStatus_FLASHIAP_AddrError :
    90       case kStatus_FLASHIAP_AddrNotMapped :
    93        case kStatus_FLASHIAP_NoPower :
    96       case kStatus_FLASHIAP_NoClock :
   110     if (result == kStatus_FLASHIAP_Success) {
   112       if (result == kStatus_FLASHIAP_Success) {
   114         if (result == kStatus_FLASHIAP_Success) {
   118             retVal = checkIAPStatus(result);
 
#define CALIBRATION_NVM_ADDR
start of final 4K (sector size) of 1M flash 
 
#define NVM_SECTOR_NUMBER
Sector number in flash where we will store parameters. 
 
#define NVM_PAGE_NUMBER
Page number in flash where we will store parameters. 
 
middleware driver for NVM on Kinetis devices 
 
The sensor_fusion.h file implements the top level programming interface. 
 
#define FLASH_SECTOR_SIZE_PROPERTY
 
byte NVM_SetBlockFlash(uint8_t *Source, uint32_t Dest, uint16_t Count)