ISSDK  1.8
IoT Sensing Software Development Kit
Macros | Functions
driver_systick.c File Reference

Encapsulates the ARM sysTick counter, which is used for benchmarking. More...

#include "sensor_fusion.h"
#include "drivers.h"
Include dependency graph for driver_systick.c:

Go to the source code of this file.

Macros

#define SYST_CSR   SysTick->CTRL
 
#define SYST_RVR   SysTick->LOAD
 
#define SYST_CVR   SysTick->VAL
 

Functions

void ARM_systick_enable (void)
 
void ARM_systick_start_ticks (int32 *pstart)
 
int32 ARM_systick_elapsed_ticks (int32 start_ticks)
 
void ARM_systick_delay_ms (uint32 iSystemCoreClock, uint32 delay_ms)
 

Detailed Description

Encapsulates the ARM sysTick counter, which is used for benchmarking.

Definition in file driver_systick.c.

Macro Definition Documentation

◆ SYST_CSR

#define SYST_CSR   SysTick->CTRL

Definition at line 17 of file driver_systick.c.

Referenced by ARM_systick_enable().

◆ SYST_CVR

#define SYST_CVR   SysTick->VAL

Definition at line 19 of file driver_systick.c.

Referenced by ARM_systick_elapsed_ticks(), and ARM_systick_start_ticks().

◆ SYST_RVR

#define SYST_RVR   SysTick->LOAD

Definition at line 18 of file driver_systick.c.

Referenced by ARM_systick_elapsed_ticks(), and ARM_systick_enable().

Function Documentation

◆ ARM_systick_delay_ms()

void ARM_systick_delay_ms ( uint32  iSystemCoreClock,
uint32  delay_ms 
)

Definition at line 54 of file driver_systick.c.

References ARM_systick_elapsed_ticks(), and ARM_systick_start_ticks().

Referenced by initializeFusionEngine().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ ARM_systick_elapsed_ticks()

int32 ARM_systick_elapsed_ticks ( int32  start_ticks)

Definition at line 43 of file driver_systick.c.

References SYST_CVR, and SYST_RVR.

Referenced by ARM_systick_delay_ms(), and fFuseSensors().

Here is the caller graph for this function:

◆ ARM_systick_enable()

void ARM_systick_enable ( void  )

Definition at line 26 of file driver_systick.c.

References SYST_CSR, and SYST_RVR.

Referenced by initializeFusionEngine().

Here is the caller graph for this function:

◆ ARM_systick_start_ticks()

void ARM_systick_start_ticks ( int32 *  pstart)

Definition at line 34 of file driver_systick.c.

References SYST_CVR.

Referenced by ARM_systick_delay_ms(), and fFuseSensors().

Here is the caller graph for this function: