17 #include "gpio_driver.h"    39     *(pWBuff) = offset | 0x80; 
    56     *(pWBuff) = offset & 0x7F; 
    60     memcpy(pWBuff + FXLS8962_SPI_CMD_LEN, pWritebuffer, size);
    76     if ((pSensorHandle == NULL) || (pBus == NULL) || (pSlaveSelect == NULL))
    97         pGPIODriver->
set_pin(pSlaveSelect);
   101         pGPIODriver->
clr_pin(pSlaveSelect);
   109     if (ARM_DRIVER_OK != status)
   136     if ((pSensorHandle == NULL) || (pRegWriteList == NULL))
   151     if (ARM_DRIVER_OK != status)
   159     if (ARM_DRIVER_OK != status)
   168     if (ARM_DRIVER_OK != status)
   183     if ((pSensorHandle == NULL) || (pReadList == NULL) || (pBuffer == NULL))
   197     if (ARM_DRIVER_OK != status)
   209     if (pSensorHandle == NULL)
   223     if (ARM_DRIVER_OK != status)
   247     if ((pSensorHandle == NULL) || (pBus == NULL))
   260     if (ARM_DRIVER_OK != status)
   291     if ((pSensorHandle == NULL) || (pRegWriteList == NULL))
   306     if (ARM_DRIVER_OK != status)
   314     if (ARM_DRIVER_OK != status)
   323     if (ARM_DRIVER_OK != status)
   338     if ((pSensorHandle == NULL) || (pReadList == NULL) || (pBuffer == NULL))
   352     if (ARM_DRIVER_OK != status)
   364     if (pSensorHandle == NULL)
   379     if (ARM_DRIVER_OK != status)
 
void(* set_pin)(pinID_t aPinId)
 
uint8_t fxls8962_spiRead_CmdBuffer[FXLS8962_SPI_MAX_MSG_SIZE]
 
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor. 
 
This structure defines the Write command List. 
 
void FXLS8962_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. 
 
uint8_t fxls8962_spiWrite_CmdDataBuffer[FXLS8962_SPI_MAX_MSG_SIZE]
 
GENERIC_DRIVER_GPIO * pGPIODriver
 
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register. 
 
int32_t Register_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t value, uint8_t mask, bool repeatedStart)
The interface function to write a sensor register. 
 
The fxls8962_drv.h file describes the FXLS8962AF driver interface and structures. ...
 
void BOARD_DELAY_ms(uint32_t delay_ms)
Function to insert delays. 
 
#define FXLS8962_SENS_CONFIG1_RST_MASK
 
int32_t FXLS8962_I2C_Initialize(fxls8962_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoami)
The interface function to initialize the sensor. 
 
void FXLS8962_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. ...
 
int32_t FXLS8962_SPI_ReadData(fxls8962_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
int32_t Register_SPI_Write(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, uint8_t offset, uint8_t value, uint8_t mask)
The interface function to write a sensor register. 
 
Access structure of the GPIO Driver. 
 
#define SPI_SS_ACTIVE_LOW
 
#define FXLS8962_SENS_CONFIG1_RST_RST
 
void(* clr_pin)(pinID_t aPinId)
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
int32_t Sensor_SPI_Read(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pReadParams, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor. 
 
This defines the sensor specific information for I2C. 
 
void FXLS8962_SPI_SetIdleTask(fxls8962_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
#define FXLS8967_WHOAMI_VALUE
 
#define FXLS8962_SPI_CMD_LEN
The size of the Sensor specific SPI Header. 
 
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
fpSpiReadPreprocessFn_t pReadPreprocessFN
 
uint8_t fxls8962_spiRead_DataBuffer[FXLS8962_SPI_MAX_MSG_SIZE]
 
The SPI Slave Transfer Command Params SDK2.0 Driver. 
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
This defines the sensor specific information for SPI. 
 
ARM_DRIVER_SPI * pCommDrv
 
int32_t FXLS8962_I2C_DeInit(fxls8962_i2c_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
int32_t FXLS8962_I2C_ReadData(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define FXLS8962_SENS_CONFIG1_ACTIVE_ACTIVE
 
#define FXLS8962_SPI_MAX_MSG_SIZE
The MAX size of SPI message. 
 
registerDeviceInfo_t deviceInfo
 
int32_t FXLS8962_SPI_Configure(fxls8962_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
ARM_DRIVER_I2C * pCommDrv
 
#define FXLS8962_SENS_CONFIG1_ACTIVE_STANDBY
 
int32_t FXLS8962_SPI_Initialize(fxls8962_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoami)
The interface function to initialize the sensor. 
 
int32_t FXLS8962_I2C_Configure(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
fpSpiWritePreprocessFn_t pWritePreprocessFN
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
This structure defines the Read command List. 
 
#define FXLS8962_SS_ACTIVE_VALUE
Is the Slave Select Pin Active Low or High. 
 
#define FXLS8974_WHOAMI_VALUE
 
#define FXLS8962_TBOOT_MAX
 
int32_t Sensor_SPI_Write(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pWriteParams, const registerwritelist_t *pRegWriteList)
Write register data to a sensor. 
 
spiSlaveSpecificParams_t slaveParams
 
void FXLS8962_I2C_SetIdleTask(fxls8962_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define FXLS8962_WHOAMI_VALUE
 
int32_t FXLS8962_SPI_Deinit(fxls8962_spi_sensorhandle_t *pSensorHandle)
The interface function to De Initialize sensor.. 
 
int32_t Register_SPI_Read(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pReadParams, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register. 
 
registeridlefunction_t idleFunction
 
#define FXLS8964_WHOAMI_VALUE
 
registerDeviceInfo_t deviceInfo
 
#define FXLS8962_SENS_CONFIG1_ACTIVE_MASK