32 #include "issdk_hal.h"    33 #include "gpio_driver.h"    40 #include "fsl_flash.h"    48 #define FXLS8471Q_SPI_CMD_LEN (2)    49 #define FXLS8471Q_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW    54 #define FXLS8962_SPI_CMD_LEN (2)    55 #define FXLS8962_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW    60 #define DIFF_P_SPI_CMD_LEN (1)    61 #define DIFF_P_SS_ACTIVE_VALUE SPI_SS_ACTIVE_LOW    66 #define MMA8491Q_WHO_AM_I (MMA8491Q_STATUS)    67 #define MMA8491Q_WHO_AM_I_VALUE                                                                                       \    68     (MMA8491Q_STATUS_RESERVED_ZERO | MMA8491Q_STATUS_XDR_DRDY | MMA8491Q_STATUS_YDR_DRDY | MMA8491Q_STATUS_ZDR_DRDY | \    69      MMA8491Q_STATUS_ZYXDR_DRDY)    71 #define ADS_QUERY_NUM (sizeof(ADS_SensorQueryList) / sizeof(sensorAccess_t))    72 #define ADS_NUM_BOARDS (sizeof(gADS_QueryMap) / ADS_QUERY_NUM)    73 #define SPI_MAX_MSG_SIZE (64)   383     "FRDM-STBC-AGM01",  
"FRDM-STBC-SA9500", 
"FRDMSTBC-A8471",   
"FRDMSTBC-A8491",
   384     "FRDMSTBC-P3115",   
"FRDMSTBI-DP300x",  
"FRDMSTBI-DP300x",  
"FRDMSTBI-B3115",
   385     "FRDM-FXS-MULT2-B", 
"FRDM-STBC-AGMP03", 
"FRDM-STBC-AGMP03", 
"FRDM-STBC-AGM04",
   386     "OnBoard",          
"OnBoard",
   415     *(pWBuff) = offset & 0x7F; 
   416     *(pWBuff + 1) = offset & 0x80;
   432     *(pWBuff) = offset | 0x80; 
   433     *(pWBuff + 1) = offset & 0x80;
   436     memcpy(pWBuff + FXLS8471Q_SPI_CMD_LEN, pWritebuffer, size);
   473     if ((ARM_DRIVER_OK != status) || (whoAmi != reg))
   492     *(pWBuff) = offset | 0x80; 
   493     *(pWBuff + 1) = 0x00;
   509     *(pWBuff) = offset & 0x7F; 
   510     *(pWBuff + 1) = 0x00;
   513     memcpy(pWBuff + FXLS8962_SPI_CMD_LEN, pWritebuffer, size);
   550     if ((ARM_DRIVER_OK != status) || (whoAmi != reg))
   569     *(pWBuff) = offset & 0x7F; 
   585     *(pWBuff) = offset | 0x80; 
   588     memcpy(pWBuff + DIFF_P_SPI_CMD_LEN, pWritebuffer, size);
   625     if ((ARM_DRIVER_OK != status) || (whoAmi != reg))
   654     partNumber = (partNumber >> 8) | (partNumber << 8);
   681     if (ARM_DRIVER_OK != status || (cmdRespHdr[1] & 0x80) != 0x80 || cmdRespHdr[2] != 
ReadVersionInfo_MMA9553[3] ||
   698     if (ARM_DRIVER_OK != status)
   700         return ARM_DRIVER_ERROR;
   704     status = 
I2CintDrv->PowerControl(ARM_POWER_FULL);
   705     if (ARM_DRIVER_OK != status)
   707         return ARM_DRIVER_ERROR;
   711     status = 
I2CintDrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   712     if (ARM_DRIVER_OK != status)
   714         return ARM_DRIVER_ERROR;
   719     if (ARM_DRIVER_OK != status)
   721         return ARM_DRIVER_ERROR;
   725     status = 
I2CextDrv->PowerControl(ARM_POWER_FULL);
   726     if (ARM_DRIVER_OK != status)
   728         return ARM_DRIVER_ERROR;
   732     status = 
I2CextDrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   733     if (ARM_DRIVER_OK != status)
   735         return ARM_DRIVER_ERROR;
   747     if (ARM_DRIVER_OK != status)
   749         return ARM_DRIVER_ERROR;
   753     status = 
SPIdrv->PowerControl(ARM_POWER_FULL);
   754     if (ARM_DRIVER_OK != status)
   756         return ARM_DRIVER_ERROR;
   761     if (ARM_DRIVER_OK != status)
   763         return ARM_DRIVER_ERROR;
   775     if (ARM_DRIVER_OK != status)
   777         return ARM_DRIVER_ERROR;
   782     if (ARM_DRIVER_OK != status)
   784         return ARM_DRIVER_ERROR;
   795     status = 
SPIdrv->Uninitialize();
   796     if (ARM_DRIVER_OK != status)
   798         return ARM_DRIVER_ERROR;
   822             if (
FXLS8962 == ADS_SensorQueryList[i].slaveAddr)
   826                     ADS_FXLS8962Query(ADS_SensorQueryList[i].whoAmIAddr, ADS_SensorQueryList[i].whoAmIValue);
   829             if (
FXLS8471 == ADS_SensorQueryList[i].slaveAddr)
   833                     ADS_FXLS8471Query(ADS_SensorQueryList[i].whoAmIAddr, ADS_SensorQueryList[i].whoAmIValue);
   836             if (
DIFF_P == ADS_SensorQueryList[i].slaveAddr)
   840                     ADS_DIFF_PQuery(ADS_SensorQueryList[i].whoAmIAddr, ADS_SensorQueryList[i].whoAmIValue);
   857             if (
FXLC95000 == ADS_SensorQueryList[i].slaveAddr)
   862             if (
MMA9553 == ADS_SensorQueryList[i].slaveAddr)
   876                                        ADS_SensorQueryList[i].whoAmIAddr, 1, ®);
   877             if ((ARM_DRIVER_OK != status) ||
   878                 ((ADS_SensorQueryList[i].whoAmIValue & ADS_SensorQueryList[i].whoAmIMask) !=
   879                  (reg & ADS_SensorQueryList[i].whoAmIMask)))
   898                                        ADS_SensorQueryList[i].whoAmIAddr, 1, ®);
   899             if ((ARM_DRIVER_OK != status) || (ADS_SensorQueryList[i].whoAmIValue != reg))
   940         status = ARM_DRIVER_OK;
   944         status = ARM_DRIVER_ERROR;
   963     if (pBoardString == NULL)
   965         return ARM_DRIVER_ERROR_PARAMETER;
   969 #ifdef SIM_SDID_FAMILYID   970     MCUInfo.
mcuFamilyId = ((SIM->SDID) & SIM_SDID_FAMILYID_MASK) >> SIM_SDID_FAMILYID_SHIFT;
   973 #ifdef SIM_SDID_SUBFAMID   974     MCUInfo.
mcuSubfamilyId = ((SIM->SDID) & SIM_SDID_SUBFAMID_MASK) >> SIM_SDID_SUBFAMID_SHIFT;
   977 #ifdef SIM_SDID_SERIESID   978     MCUInfo.
mcuSeriesId = ((SIM->SDID) & SIM_SDID_SERIESID_MASK) >> SIM_SDID_SERIESID_SHIFT;
   981 #ifdef SIM_SDID_FAMID   982     MCUInfo.
mcuFamId = ((SIM->SDID) & SIM_SDID_FAMID_MASK) >> SIM_SDID_FAMID_SHIFT;
   985     MCUInfo.
mcuPinId = ((SIM->SDID) & SIM_SDID_PINID_MASK) >> SIM_SDID_PINID_SHIFT;
  1001     status = ARM_DRIVER_OK;
  1003     switch (MCUInfo.
board)
  1006             strncpy(pBoardString, 
"FRDM-KW41Z", bufferLength);
  1009             strncpy(pBoardString, 
"FRDM-KE15Z", bufferLength);
  1012             strncpy(pBoardString, 
"FRDM-KL25Z", bufferLength);
  1015             strncpy(pBoardString, 
"FRDM-KL27Z", bufferLength);
  1018             strncpy(pBoardString, 
"FRDM-K22F", bufferLength);
  1021             strncpy(pBoardString, 
"FRDM-K64F", bufferLength);
  1024             strncpy(pBoardString, 
"RD-KL25-AGMP01", bufferLength);
  1027             status = ARM_DRIVER_ERROR;
  1047         status = strncmp((
char *)pResultString, (
char *)pRecord->
ADSString, pRecord->
length);
  1063     uint32_t pflashSectorSize = 0;
  1066     flash_config_t s_flashDriver;
  1070     flashRecord.
length = strlen((
char const *)pResultString);
  1074     memset(&s_flashDriver, 0, 
sizeof(flash_config_t));
  1077     result = FLASH_Init(&s_flashDriver);
  1078     if (kStatus_FLASH_Success == result)
  1084         result = FLASH_Erase(&s_flashDriver, 
ADS_NVM_ADDR, pflashSectorSize, kFLASH_ApiEraseKey);
  1085         if (kStatus_FLASH_Success == result)
  1088             result = FLASH_Program(&s_flashDriver, 
ADS_NVM_ADDR, (uint8_t *)&flashRecord,
  1089                                    sizeof(flashRecord)); 
  1090             if (kStatus_FLASH_Success == result)
  1107     if (ARM_DRIVER_ERROR == status)
  1109         strncpy(boardString, 
"NotDetected", bufferLength);
  1114     if (ARM_DRIVER_ERROR == status)
  1116         strncpy(shieldString, 
"NotDetected", bufferLength);
  1122     position = strlen(appName);
  1124     finalString[position++] = 
':';
  1127     position += strlen(shieldString);
  1136         strcpy(finalString, shieldString);
  1137         snprintf(shieldString, bufferLength, 
"Changed:%s", finalString);
 #define MMA9553_HDR_SIZE
Size of fixed header bytes in sensor commands. 
 
void(* set_pin)(pinID_t aPinId)
 
#define FXAS21002_WHO_AM_I_WHOAMI_PROD_VALUE
 
char ADSString[ADS_FLASH_STRING_LENGTH]
 
The mma845x.h contains the MMA845x sensor register definitions and its bit mask. 
 
const sensorAccess_t ADS_SensorQueryList[]
This constant data structure contains the expected valid comm/sensor/who_am_i combinations. 
 
#define MMA8451_WHO_AM_I_WHOAMI_VALUE
 
#define I2C_BB_DEVICE_INDEX
 
ADS_FlashStatus_t ADS_FlashCompare(char *pResultString)
 
This structure defines the device specific info required by register I/O. 
 
spiSlaveSpecificParams_t spiParams_diff_p
 
ADS_Status_t ADS_FXLC95000Query()
 
The fxls8471q.h file contains the register definitions for fxls8471q sensor driver. 
 
#define MMA8491Q_WHO_AM_I_VALUE
 
#define I2C_S1_DEVICE_INDEX
 
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register. 
 
void BOARD_DELAY_ms(uint32_t delay_ms)
Function to insert delays. 
 
#define FXOS8700_WHO_AM_I_PROD_VALUE
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
spiSlaveSpecificParams_t spiParams_8471
 
The register_io_spi.h file declares low-level interface functions for reading and writing sensor regi...
 
uint8_t spiRead_CmdBuffer[SPI_MAX_MSG_SIZE]
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
This structure defines the spi slave command format. 
 
#define FXLC95000_PART_NUMBER_OFFSET
Offset of 2-Byte SA95000 Part Number in Device Info Response. 
 
Access structure of the GPIO Driver. 
 
#define FXLC95000_I2C_ADDR
 
#define ADS_FLASH_STRING_LENGTH
 
#define SPI_SS_ACTIVE_LOW
 
ADS_FlashStatus_t
This enumeration defines the ADS Flash storage status. 
 
This defines a record type to store ADS results string in Flash memory. 
 
ARM_DRIVER_I2C * I2CextDrv
 
void ADS_DIFF_P_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
 
#define MMA8491Q_WHO_AM_I
These variables are specific to MMA8491Q which does not have a Who Am I register. ...
 
void ADS_InitSPI_FXLS8471()
 
#define FXLS8471Q_WHO_AM_I_WHOAMI_VALUE
 
#define FXLS8962_SPI_CMD_LEN
These variables are specific to SPI access to the FXLS8962 for ADS. 
 
void(* clr_pin)(pinID_t aPinId)
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
#define SPI_S_BAUDRATE
Transfer baudrate - 500k. 
 
#define DIFF_P_SPI_CMD_LEN
These variables are specific to SPI access to the DIFF_P for ADS. 
 
#define SPI_S_DEVICE_INDEX
 
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
 
void ADS_DIFF_P_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 
This defines a record type to store the communication channel info and WHO_AM_I address/value for var...
 
ADS_Status_t ADS_MMA9553Query()
 
uint8_t spiWrite_CmdDataBuffer[SPI_MAX_MSG_SIZE]
 
fpSpiReadPreprocessFn_t pReadPreprocessFN
 
The fxas21002.h contains the fxas21002 sensor register definitions and its bit mask. 
 
The SPI Slave Transfer Command Params SDK2.0 Driver. 
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define FXAS21002_I2C_ADDR
 
#define ADS_NVM_ADDR
start of the next to last 4K (sector size) of the 1M flash 
 
GENERIC_DRIVER_GPIO * pGPIODriver
 
#define MMA8491Q_T_ON_TYPICAL
 
ARM_DRIVER_I2C * I2CintDrv
 
#define FXLS8471Q_SS_ACTIVE_VALUE
 
#define MMA8491Q_I2C_ADDRESS
 
#define FLASH_SECTOR_SIZE_PROPERTY
 
ADS_Status_t ADS_FXLS8471Query(uint8_t whoAmiAddr, uint8_t whoAmi)
 
This defines a record type to store the expected field values in the MCU SDID register word aligned...
 
int ADS_DetectFRDM(char *pBoardString, size_t bufferLength)
 
ADS_Status_t ADS_DIFF_PQuery(uint8_t whoAmiAddr, uint8_t whoAmi)
 
const mcuSDID_t ADS_ValidSDIDValues[]
This constant data structure contains the expected valid MCU SDID combinations. 
 
int ADS_DetectShield(char *pShieldString, size_t bufferLength)
 
#define ADS_NO_SHIELD_DETECTED
 
void ADS_FXLS8471Q_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
 
#define FXLS8962_SS_ACTIVE_VALUE
 
void ADS_InitSPI_DIFF_P()
 
spiSlaveSpecificParams_t spiParams_8962
 
#define I2C_S1_SIGNAL_EVENT
 
const ADS_Status_t gADS_QueryMap[][ADS_QUERY_NUM]
These are the expected query signatures for the shield boards. 
 
void ADS_FXLS8962_SPI_ReadPreprocess(void *pCmdOut, uint32_t offset, uint32_t size)
 
void ADS_InitSPI_FXLS8962()
 
char ADS_ShieldList[][ADS_MAX_STRING_LENGTH]
 
ADS_SupportedBoards_t board
 
#define FXLS8471Q_SPI_CMD_LEN
These variables are specific to SPI access to the FXLS8471 for ADS. 
 
int32_t Register_I2C_BlockWrite(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, const uint8_t *pBuffer, uint8_t bytesToWrite)
The interface function to write a sensor register. 
 
#define ADS_MAX_STRING_LENGTH
 
#define DIFF_P_SS_ACTIVE_VALUE
 
#define FXLC95000_PART_NUMBER_SIZE
The FXLC95000 Size of Part Number. 
 
ADS_Status_t ADS_FXLS8962Query(uint8_t whoAmiAddr, uint8_t whoAmi)
 
#define FXPQ3115_WHOAMI_VALUE
 
uint8_t spiRead_DataBuffer[SPI_MAX_MSG_SIZE]
 
ARM_DRIVER_SPI * SPIdrv
These values hold the ARM CMSIS Driver interface pointers. 
 
#define MMA8491Q_STATUS_RESERVED_MASK
 
#define MPL3115_WHOAMI_VALUE
 
char boardString[ADS_MAX_STRING_LENGTH]
 
#define FXLC95000_PART_NUMBER
The FXLC95000 2-byte packed BCD encoded Part Number (BCD for Last 4 characters). 
 
fpSpiWritePreprocessFn_t pWritePreprocessFN
 
The auto_detection_shield.h file describes the definitions for Sensor I2C and SPI parameters required...
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define MAG3110_WHOAMI_VALUE
 
#define I2C_BB_SIGNAL_EVENT
 
#define FXPQ3115_I2C_ADDR
 
void ADS_FXLS8471Q_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 
enum ADS_Status ADS_Status_t
This defines the return status. 
 
void ADS_FXLS8962_SPI_WritePreprocess(void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 
#define SPI_S_SIGNAL_EVENT
 
This file contains the FXLS8962 Accelerometer register definitions, access macros, and device access functions. 
 
const uint8_t ReadVersionInfo_MMA9553[4]
The Read Version Info Command for FXLC95000. 
 
#define FXLS8962_I2C_ADDR
 
The fxos8700.h file contains the register definitions for FXOS8700 sensor driver. ...
 
#define FXLS8962_WHOAMI_VALUE
 
#define MMA8652_WHOAMI_VALUE
 
#define FXOS8700_I2C_ADDR
 
int32_t Register_SPI_Read(ARM_DRIVER_SPI *pCommDrv, registerDeviceInfo_t *devInfo, void *pReadParams, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register. 
 
ADS_Status_t ADS_FlashUpdate(char *pResultString)
 
ADS_Status_t gADS_QueryResults[ADS_QUERY_NUM]
This global contains the results from the sensor query.