![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|


Go to the source code of this file.
Macros | |
| #define | BOARD_NAME "LPCXPRESSO54114" |
| The board name. More... | |
| #define | BOARD_EXTCLKINRATE (0) |
| #define | BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_FLEXCOMM |
| The UART to use for debug messages. More... | |
| #define | BOARD_DEBUG_UART_BASEADDR (uint32_t) USART0 |
| #define | BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetFreq(kCLOCK_Flexcomm0) |
| #define | BOARD_DEBUG_UART_CLK_ATTACH kFRO12M_to_FLEXCOMM0 |
| #define | BOARD_DEBUG_UART_RST kFC0_RST_SHIFT_RSTn |
| #define | BOARD_DEBUG_SPI_CLK_FREQ 12000000 |
| #define | BOARD_DEBUG_UART_BAUDRATE 115200 |
| #define | BOARD_LED_RED_GPIO GPIO |
| #define | BOARD_LED_RED_GPIO_PORT 0U |
| #define | BOARD_LED_RED_GPIO_PIN 29U |
| #define | BOARD_LED_GREEN_GPIO GPIO |
| #define | BOARD_LED_GREEN_GPIO_PORT 1U |
| #define | BOARD_LED_GREEN_GPIO_PIN 10U |
| #define | BOARD_LED_BLUE_GPIO GPIO |
| #define | BOARD_LED_BLUE_GPIO_PORT 1U |
| #define | BOARD_LED_BLUE_GPIO_PIN 9U |
| #define | BOARD_SW1_GPIO GPIO |
| #define | BOARD_SW1_GPIO_PORT 0U |
| #define | BOARD_SW1_GPIO_PIN 24U |
| #define | BOARD_SW1_NAME "SW1" |
| #define | BOARD_SW3_IRQ PIN_INT0_IRQn |
| #define | BOARD_SW3_IRQ_HANDLER PIN_INT0_IRQHandler |
| #define | BOARD_SW2_GPIO GPIO |
| #define | BOARD_SW2_GPIO_PORT 0U |
| #define | BOARD_SW2_GPIO_PIN 31U |
| #define | BOARD_SW2_NAME "SW2" |
| #define | BOARD_SW3_IRQ PIN_INT0_IRQn |
| #define | BOARD_SW3_IRQ_HANDLER PIN_INT0_IRQHandler |
| #define | BOARD_SW3_GPIO GPIO |
| #define | BOARD_SW3_GPIO_PORT 0U |
| #define | BOARD_SW3_GPIO_PIN 4U |
| #define | BOARD_SW3_NAME "SW3" |
| #define | BOARD_SW3_IRQ PIN_INT0_IRQn |
| #define | BOARD_SW3_IRQ_HANDLER PIN_INT0_IRQHandler |
| #define | BOARD_SW3_GPIO_PININT_INDEX 0 |
| #define | LOGIC_LED_ON 0U |
| #define | LOGIC_LED_OFF 1U |
| #define | LED_RED_INIT(output) |
| #define | LED_RED_ON() |
| #define | LED_RED_OFF() |
| #define | LED_RED_TOGGLE() |
| #define | LED_GREEN_INIT(output) |
| #define | LED_GREEN_ON() |
| #define | LED_GREEN_OFF() |
| #define | LED_GREEN_TOGGLE() |
| #define | LED_BLUE_INIT(output) |
| #define | LED_BLUE_ON() |
| #define | LED_BLUE_OFF() |
| #define | LED_BLUE_TOGGLE() |
Functions | |
| status_t | BOARD_InitDebugConsole (void) |
| #define BOARD_DEBUG_UART_CLK_ATTACH kFRO12M_to_FLEXCOMM0 |
Definition at line 28 of file board.h.
Referenced by BOARD_InitDebugConsole(), initializeControlPort(), and USART0_InitPins().
| #define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetFreq(kCLOCK_Flexcomm0) |
| #define BOARD_DEBUG_UART_RST kFC0_RST_SHIFT_RSTn |
Definition at line 29 of file board.h.
Referenced by BOARD_InitDebugConsole().
| #define BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_FLEXCOMM |
| #define LED_BLUE_INIT | ( | output | ) |
Enable target LED_BLUE
| #define LED_BLUE_OFF | ( | ) |
Turn off target LED_BLUE
| #define LED_BLUE_ON | ( | ) |
Turn on target LED_BLUE
| #define LED_BLUE_TOGGLE | ( | ) |
Toggle on target LED_BLUE
| #define LED_GREEN_INIT | ( | output | ) |
Enable target LED_GREEN
| #define LED_GREEN_OFF | ( | ) |
Turn off target LED_GREEN
| #define LED_GREEN_ON | ( | ) |
Turn on target LED_GREEN
| #define LED_GREEN_TOGGLE | ( | ) |
Toggle on target LED_GREEN
| #define LED_RED_INIT | ( | output | ) |
Enable target LED_RED
| #define LED_RED_OFF | ( | ) |
Turn off target LED_RED
| #define LED_RED_ON | ( | ) |
Turn on target LED_RED
| #define LED_RED_TOGGLE | ( | ) |
Toggle on target LED_RED