|
| #define | BOARD_NAME "FRDM-K32W042" |
| | The board name. More...
|
| |
| #define | BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_LPUART |
| |
| #define | BOARD_DEBUG_UART_BAUDRATE 115200U |
| |
| #define | BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART0 |
| |
| #define | BOARD_DEBUG_UART_INSTANCE 0U |
| |
| #define | BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetIpFreq(kCLOCK_Lpuart0) |
| |
| #define | BOARD_UART_IRQ LPUART0_IRQn |
| |
| #define | BOARD_UART_IRQ_HANDLER LPUART0_IRQHandler |
| |
| #define | MU_IRQ_PRIORITY (2) |
| |
| #define | BOARD_SW2_GPIO GPIOA |
| | Define the port interrupt number for the board switches. More...
|
| |
| #define | BOARD_SW2_PORT PORTA |
| |
| #define | BOARD_SW2_GPIO_PIN 0U |
| |
| #define | BOARD_SW2_IRQ PORTA_IRQn |
| |
| #define | BOARD_SW2_IRQ_HANDLER PORTA_IRQHandler |
| |
| #define | BOARD_SW2_NAME "SW2" |
| |
| #define | BOARD_LED_RED_GPIO GPIOA |
| |
| #define | BOARD_LED_RED_GPIO_PIN 24U |
| |
| #define | BOARD_TPM_CHANNEL 0U |
| | The TPM channel used for board. More...
|
| |
| #define | LOGIC_LED_ON 1U |
| |
| #define | LOGIC_LED_OFF 0U |
| |
| #define | BOARD_LED1_GPIO GPIOA |
| |
| #define | BOARD_LED1_GPIO_PIN 24U |
| |
| #define | BOARD_LED2_GPIO GPIOA |
| |
| #define | BOARD_LED2_GPIO_PIN 23U |
| |
| #define | BOARD_LED3_GPIO GPIOA |
| |
| #define | BOARD_LED3_GPIO_PIN 22U |
| |
| #define | LED1_INIT(output) |
| |
| #define | LED1_ON() GPIO_SetPinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN) |
| |
| #define | LED1_OFF() GPIO_ClearPinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN) |
| |
| #define | LED1_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN) |
| |
| #define | LED2_INIT(output) |
| |
| #define | LED2_ON() GPIO_SetPinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN) |
| |
| #define | LED2_OFF() GPIO_ClearPinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN) |
| |
| #define | LED2_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN) |
| |
| #define | LED3_INIT(output) |
| |
| #define | LED3_ON() GPIO_SetPinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN) |
| |
| #define | LED3_OFF() GPIO_ClearPinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN) |
| |
| #define | LED3_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN) |
| |
| #define | BOARD_USDHC0_BASEADDR USDHC0 |
| |
| #define | BOARD_USDHC_CD_PORT_BASE PORTC |
| |
| #define | BOARD_USDHC_CD_GPIO_BASE GPIOC |
| |
| #define | BOARD_USDHC_CD_GPIO_PIN 27 |
| |
| #define | BOARD_USDHC_CD_PORT_IRQ PORTC_IRQn |
| |
| #define | BOARD_USDHC_CD_PORT_IRQ_HANDLER PORTC_IRQHandler |
| |
| #define | BOARD_USDHC_CD_GPIO_INIT() |
| |
| #define | BOARD_USDHC_CD_STATUS() (GPIO_ReadPinInput(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN)) |
| |
| #define | BOARD_USDHC_CD_INTERRUPT_STATUS() (GPIO_GetPinsInterruptFlags(BOARD_USDHC_CD_GPIO_BASE)) |
| |
| #define | BOARD_USDHC_CD_CLEAR_INTERRUPT(flag) (GPIO_ClearPinsInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, flag)) |
| |
| #define | BOARD_USDHC_CARD_INSERT_CD_LEVEL (1U) |
| |
| #define | BOARD_USDHC0_CLK_FREQ (CLOCK_GetIpFreq(kCLOCK_Sdhc0)) |
| |
| #define | BOARD_SD_HOST_BASEADDR BOARD_USDHC0_BASEADDR |
| |
| #define | BOARD_SD_HOST_CLK_FREQ BOARD_USDHC0_CLK_FREQ |
| |
| #define | BOARD_SD_HOST_IRQ USDHC0_IRQn |
| |
| #define | BOARD_SD_SUPPORT_180V (0U) |
| |
| #define | BOARD_MMC_HOST_BASEADDR BOARD_USDHC0_BASEADDR |
| |
| #define | BOARD_MMC_HOST_CLK_FREQ BOARD_USDHC0_CLK_FREQ |
| |
| #define | BOARD_MMC_HOST_IRQ USDHC0_IRQn |
| |
| #define | BOARD_MMC_VCCQ_SUPPLY kMMC_VoltageWindows270to360 |
| |
| #define | BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360 |
| |
| #define | BOARD_MMC_PIN_CONFIG(speed, strength) |
| |
| #define | BOARD_SD_POWER_RESET_GPIO () |
| |
| #define | BOARD_SD_POWER_RESET_GPIO_PIN () |
| |
| #define | BOARD_USDHC_SDCARD_POWER_CONTROL_INIT() |
| |
| #define | BOARD_USDHC_SDCARD_POWER_CONTROL(state) |
| |
| #define | BOARD_SD_PIN_CONFIG(speed, strength) |
| |
| #define | BOARD_USDHC_MMCCARD_POWER_CONTROL(enable) |
| |
| #define | BOARD_USDHC_MMCCARD_POWER_CONTROL_INIT() |
| |
| #define | LLWU_SW_GPIO BOARD_SW2_GPIO |
| |
| #define | LLWU_SW_PORT BOARD_SW2_PORT |
| |
| #define | LLWU_SW_GPIO_PIN BOARD_SW2_GPIO_PIN |
| |
| #define | LLWU_SW_IRQ BOARD_SW2_IRQ |
| |
| #define | LLWU_SW_IRQ_HANDLER BOARD_SW2_IRQ_HANDLER |
| |
| #define | LLWU_SW_NAME BOARD_SW2_NAME |
| |
| #define | BOARD_SPI_FLASH_CS_GPIO GPIOB |
| |
| #define | BOARD_SPI_FLASH_CS_GPIO_PIN 22U |
| |