19 #define BOARD_NAME "FRDM-K32W042"    22 #define BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_LPUART    23 #define BOARD_DEBUG_UART_BAUDRATE 115200U    24 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART0    25 #define BOARD_DEBUG_UART_INSTANCE    0U    26 #define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetIpFreq(kCLOCK_Lpuart0)    27 #define BOARD_UART_IRQ LPUART0_IRQn    28 #define BOARD_UART_IRQ_HANDLER LPUART0_IRQHandler    31 #if defined(FSL_FEATURE_MU_SIDE_A)    33 #define MU_IRQ MUA_IRQn    34 #define MU_IRQ_HANDLER MUA_IRQHandler    36 #if defined(FSL_FEATURE_MU_SIDE_B)    38 #define MU_IRQ MUB_IRQn    39 #define MU_IRQ_HANDLER MUB_IRQHandler    41 #define MU_IRQ_PRIORITY (2)    44 #define BOARD_SW2_GPIO GPIOA    45 #define BOARD_SW2_PORT PORTA    46 #define BOARD_SW2_GPIO_PIN 0U    47 #define BOARD_SW2_IRQ PORTA_IRQn    48 #define BOARD_SW2_IRQ_HANDLER PORTA_IRQHandler    49 #define BOARD_SW2_NAME "SW2"    52 #define BOARD_LED_RED_GPIO GPIOA    53 #define BOARD_LED_RED_GPIO_PIN 24U    56 #define BOARD_TPM_CHANNEL 0U    58 #define LOGIC_LED_ON 1U    59 #define LOGIC_LED_OFF 0U    60 #define BOARD_LED1_GPIO GPIOA    61 #define BOARD_LED1_GPIO_PIN 24U    62 #define BOARD_LED2_GPIO GPIOA    63 #define BOARD_LED2_GPIO_PIN 23U    64 #define BOARD_LED3_GPIO GPIOA    65 #define BOARD_LED3_GPIO_PIN 22U    67 #define LED1_INIT(output)                                              \    68     GPIO_WritePinOutput(BOARD_LED1_GPIO, BOARD_LED1_GPIO_PIN, output); \    69     BOARD_LED1_GPIO->PDDR |= (1U << BOARD_LED1_GPIO_PIN)                                    70 #define LED1_ON() GPIO_SetPinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN)            71 #define LED1_OFF() GPIO_ClearPinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN)         72 #define LED1_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED1_GPIO, 1U << BOARD_LED1_GPIO_PIN)     74 #define LED2_INIT(output)                                              \    75     GPIO_WritePinOutput(BOARD_LED2_GPIO, BOARD_LED2_GPIO_PIN, output); \    76     BOARD_LED2_GPIO->PDDR |= (1U << BOARD_LED2_GPIO_PIN)                                    77 #define LED2_ON() GPIO_SetPinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN)            78 #define LED2_OFF() GPIO_ClearPinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN)         79 #define LED2_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED2_GPIO, 1U << BOARD_LED2_GPIO_PIN)     81 #define LED3_INIT(output)                                              \    82     GPIO_WritePinOutput(BOARD_LED3_GPIO, BOARD_LED3_GPIO_PIN, output); \    83     BOARD_LED3_GPIO->PDDR |= (1U << BOARD_LED3_GPIO_PIN)                                    84 #define LED3_ON() GPIO_SetPinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN)            85 #define LED3_OFF() GPIO_ClearPinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN)         86 #define LED3_TOGGLE() GPIO_TogglePinsOutput(BOARD_LED3_GPIO, 1U << BOARD_LED3_GPIO_PIN)     88 #define BOARD_USDHC0_BASEADDR USDHC0    89 #define BOARD_USDHC_CD_PORT_BASE PORTC    90 #define BOARD_USDHC_CD_GPIO_BASE GPIOC    91 #define BOARD_USDHC_CD_GPIO_PIN 27    92 #define BOARD_USDHC_CD_PORT_IRQ PORTC_IRQn    93 #define BOARD_USDHC_CD_PORT_IRQ_HANDLER PORTC_IRQHandler    95 #define BOARD_USDHC_CD_GPIO_INIT()                                                                                \    97         gpio_pin_config_t sw_config = {kGPIO_DigitalInput, 0};                                                    \    98         GPIO_PinInit(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN, &sw_config);                              \    99         PORT_SetPinInterruptConfig(BOARD_USDHC_CD_PORT_BASE, BOARD_USDHC_CD_GPIO_PIN, kPORT_InterruptRisingEdge); \   102 #define BOARD_USDHC_CD_STATUS() (GPIO_ReadPinInput(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN))   104 #define BOARD_USDHC_CD_INTERRUPT_STATUS() (GPIO_GetPinsInterruptFlags(BOARD_USDHC_CD_GPIO_BASE))   105 #define BOARD_USDHC_CD_CLEAR_INTERRUPT(flag) (GPIO_ClearPinsInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, flag))   106 #define BOARD_USDHC_CARD_INSERT_CD_LEVEL (1U)   107 #define BOARD_USDHC0_CLK_FREQ (CLOCK_GetIpFreq(kCLOCK_Sdhc0))   109 #define BOARD_SD_HOST_BASEADDR BOARD_USDHC0_BASEADDR   110 #define BOARD_SD_HOST_CLK_FREQ BOARD_USDHC0_CLK_FREQ   111 #define BOARD_SD_HOST_IRQ USDHC0_IRQn   112 #define BOARD_SD_SUPPORT_180V (0U)   113 #define BOARD_MMC_HOST_BASEADDR BOARD_USDHC0_BASEADDR   114 #define BOARD_MMC_HOST_CLK_FREQ BOARD_USDHC0_CLK_FREQ   115 #define BOARD_MMC_HOST_IRQ USDHC0_IRQn   116 #define BOARD_MMC_VCCQ_SUPPLY kMMC_VoltageWindows270to360   117 #define BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360   118 #define BOARD_MMC_PIN_CONFIG(speed, strength)   121 #define BOARD_SD_POWER_RESET_GPIO ()   122 #define BOARD_SD_POWER_RESET_GPIO_PIN ()   123 #define BOARD_USDHC_SDCARD_POWER_CONTROL_INIT()   124 #define BOARD_USDHC_SDCARD_POWER_CONTROL(state)   125 #define BOARD_SD_PIN_CONFIG(speed, strength)   126 #define BOARD_USDHC_MMCCARD_POWER_CONTROL(enable)   127 #define BOARD_USDHC_MMCCARD_POWER_CONTROL_INIT()   129 #define LLWU_SW_GPIO BOARD_SW2_GPIO   130 #define LLWU_SW_PORT BOARD_SW2_PORT   131 #define LLWU_SW_GPIO_PIN BOARD_SW2_GPIO_PIN   132 #define LLWU_SW_IRQ BOARD_SW2_IRQ   133 #define LLWU_SW_IRQ_HANDLER BOARD_SW2_IRQ_HANDLER   134 #define LLWU_SW_NAME BOARD_SW2_NAME   136 #define BOARD_SPI_FLASH_CS_GPIO GPIOB   137 #define BOARD_SPI_FLASH_CS_GPIO_PIN 22U   138 #if defined(__cplusplus)   148 #if defined(__cplusplus) void BOARD_InitDebugConsole(void)