ISSDK  1.8
IoT Sensing Software Development Kit
board.h
Go to the documentation of this file.
1 /*
2  * Copyright 2018 NXP
3  * All rights reserved.
4  *
5  * SPDX-License-Identifier: BSD-3-Clause
6  */
7 
8 #ifndef _BOARD_H_
9 #define _BOARD_H_
10 
11 #include "clock_config.h"
12 #include "fsl_common.h"
13 #include "fsl_gpio.h"
14 #include "fsl_clock.h"
15 
16 /*******************************************************************************
17  * Definitions
18  ******************************************************************************/
19 /*! @brief The board name */
20 #define BOARD_NAME "MIMXRT1170-EVK"
21 #ifndef DEBUG_CONSOLE_UART_INDEX
22 #define DEBUG_CONSOLE_UART_INDEX 1
23 #endif
24 
25 /* The UART to use for debug messages. */
26 #define BOARD_DEBUG_UART_TYPE kSerialPort_Uart
27 #define BOARD_DEBUG_UART_CLK_FREQ 24000000
28 
29 #if DEBUG_CONSOLE_UART_INDEX == 1
30 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART1
31 #define BOARD_DEBUG_UART_INSTANCE 1U
32 #define BOARD_UART_IRQ LPUART1_IRQn
33 #define BOARD_UART_IRQ_HANDLER LPUART1_IRQHandler
34 #elif DEBUG_CONSOLE_UART_INDEX == 2
35 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART2
36 #define BOARD_DEBUG_UART_INSTANCE 2U
37 #define BOARD_UART_IRQ LPUART2_IRQn
38 #define BOARD_UART_IRQ_HANDLER LPUART2_IRQHandler
39 #elif DEBUG_CONSOLE_UART_INDEX == 12
40 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART12
41 #define BOARD_DEBUG_UART_INSTANCE 12U
42 #define BOARD_UART_IRQ LPUART12_IRQn
43 #define BOARD_UART_IRQ_HANDLER LPUART12_IRQHandler
44 #else
45 #error "Unsupported UART"
46 #endif
47 
48 #ifndef BOARD_DEBUG_UART_BAUDRATE
49 #define BOARD_DEBUG_UART_BAUDRATE (115200U)
50 #endif /* BOARD_DEBUG_UART_BAUDRATE */
51 
52 /* Definitions for eRPC MU transport layer */
53 #if defined(FSL_FEATURE_MU_SIDE_A)
54 #define MU_BASE MUA
55 #define MU_IRQ MUA_IRQn
56 #define MU_IRQ_HANDLER MUA_IRQHandler
57 #endif
58 #if defined(FSL_FEATURE_MU_SIDE_B)
59 #define MU_BASE MUB
60 #define MU_IRQ MUB_IRQn
61 #define MU_IRQ_HANDLER MUB_IRQHandler
62 #endif
63 #define MU_IRQ_PRIORITY (2)
64 
65 /*! @brief The USER_LED used for board */
66 #define LOGIC_LED_ON (0U)
67 #define LOGIC_LED_OFF (1U)
68 #ifndef BOARD_USER_LED_GPIO
69 #define BOARD_USER_LED_GPIO GPIO9
70 #endif
71 #ifndef BOARD_USER_LED_GPIO_PIN
72 #define BOARD_USER_LED_GPIO_PIN (3U)
73 #endif
74 
75 #define USER_LED_INIT(output) \
76  GPIO_PinWrite(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN, output); \
77  BOARD_USER_LED_GPIO->GDIR |= (1U << BOARD_USER_LED_GPIO_PIN) /*!< Enable target USER_LED */
78 #define USER_LED_OFF() \
79  GPIO_PortClear(BOARD_USER_LED_GPIO, 1U << BOARD_USER_LED_GPIO_PIN) /*!< Turn off target USER_LED */
80 #define USER_LED_ON() GPIO_PortSet(BOARD_USER_LED_GPIO, 1U << BOARD_USER_LED_GPIO_PIN) /*!<Turn on target USER_LED*/
81 #define USER_LED_TOGGLE() \
82  GPIO_PinWrite(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN, \
83  0x1 ^ GPIO_PinRead(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN)) /*!< Toggle target USER_LED */
84 
85 /*! @brief Define the port interrupt number for the board switches */
86 #ifndef BOARD_USER_BUTTON_GPIO
87 #define BOARD_USER_BUTTON_GPIO GPIO13
88 #endif
89 #ifndef BOARD_USER_BUTTON_GPIO_PIN
90 #define BOARD_USER_BUTTON_GPIO_PIN (0U)
91 #endif
92 #define BOARD_USER_BUTTON_IRQ GPIO13_Combined_0_31_IRQn
93 #define BOARD_USER_BUTTON_IRQ_HANDLER GPIO13_Combined_0_31_IRQHandler
94 #define BOARD_USER_BUTTON_NAME "SW7"
95 
96 /*! @brief The board flash size */
97 #define BOARD_FLASH_SIZE (0x1000000U)
98 
99 /* SKIP_SEMC_INIT can also be defined independently */
100 #ifdef USE_SDRAM
101 #define SKIP_SEMC_INIT
102 #endif
103 
104 /*! @brief The ENET PHY address. */
105 #define BOARD_ENET0_PHY_ADDRESS (0x02U) /* Phy address of enet port 0. */
106 
107 /* @brief The EMVSIM SMARTCARD PHY configuration. */
108 #define BOARD_SMARTCARD_MODULE (EMVSIM1) /*!< SMARTCARD communicational module instance */
109 #define BOARD_SMARTCARD_MODULE_IRQ (EMVSIM1_IRQn) /*!< SMARTCARD communicational module IRQ handler */
110 #define BOARD_SMARTCARD_CLOCK_MODULE_CLK_FREQ (CLOCK_GetRootClockFreq(kCLOCK_Root_Emv1))
111 #define BOARD_SMARTCARD_CLOCK_VALUE (4000000U) /*!< SMARTCARD clock frequency */
112 
113 /* USB PHY condfiguration */
114 #define BOARD_USB_PHY_D_CAL (0x0CU)
115 #define BOARD_USB_PHY_TXCAL45DP (0x06U)
116 #define BOARD_USB_PHY_TXCAL45DM (0x06U)
117 
118 #define BOARD_ARDUINO_INT_IRQ (GPIO1_INT3_IRQn)
119 #define BOARD_ARDUINO_I2C_IRQ (LPI2C1_IRQn)
120 #define BOARD_ARDUINO_I2C_INDEX (1)
121 #define BOARD_USDHC1_BASEADDR USDHC1
122 #define BOARD_USDHC2_BASEADDR USDHC2
123 #define BOARD_USDHC_CD_GPIO_BASE GPIO9
124 #define BOARD_USDHC_CD_GPIO_PIN 2
125 #define BOARD_USDHC_CD_PORT_IRQ GPIO2_Combined_16_31_IRQn
126 #define BOARD_USDHC_CD_PORT_IRQ_HANDLER GPIO2_Combined_16_31_IRQHandler
128 #define BOARD_USDHC_CD_STATUS() (GPIO_PinRead(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN))
130 #define BOARD_USDHC_CD_INTERRUPT_STATUS() (GPIO_PortGetInterruptFlags(BOARD_USDHC_CD_GPIO_BASE))
131 #define BOARD_USDHC_CD_CLEAR_INTERRUPT(flag) (GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, flag))
132 
133 #define BOARD_USDHC_CD_GPIO_INIT() \
134  { \
135  gpio_pin_config_t sw_config = { \
136  kGPIO_DigitalInput, \
137  0, \
138  kGPIO_IntRisingOrFallingEdge, \
139  }; \
140  GPIO_PinInit(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN, &sw_config); \
141  GPIO_PortEnableInterrupts(BOARD_USDHC_CD_GPIO_BASE, 1U << BOARD_USDHC_CD_GPIO_PIN); \
142  GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, ~0); \
143  }
144 #define BOARD_HAS_SDCARD (1U)
145 #define BOARD_SD_POWER_RESET_GPIO (GPIO9)
146 #define BOARD_SD_POWER_RESET_GPIO_PIN (14U)
147 
148 #define BOARD_USDHC_CARD_INSERT_CD_LEVEL (0U)
150 #define BOARD_USDHC_MMCCARD_POWER_CONTROL(state)
152 #define BOARD_USDHC_MMCCARD_POWER_CONTROL_INIT() \
153  { \
154  gpio_pin_config_t sw_config = { \
155  kGPIO_DigitalOutput, \
156  0, \
157  kGPIO_NoIntmode, \
158  }; \
159  GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \
160  GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, true); \
161  }
162 
163 #define BOARD_USDHC_SDCARD_POWER_CONTROL_INIT() \
164  { \
165  gpio_pin_config_t sw_config = { \
166  kGPIO_DigitalOutput, \
167  0, \
168  kGPIO_NoIntmode, \
169  }; \
170  GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \
171  }
172 
173 #define BOARD_USDHC_SDCARD_POWER_CONTROL(state) \
174  (GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, state == true ? false : true))
175 
176 #define BOARD_USDHC1_CLK_FREQ 400000000U
177 #define BOARD_USDHC2_CLK_FREQ (CLOCK_GetSysPfdFreq(kCLOCK_Pfd0) / (CLOCK_GetDiv(kCLOCK_Usdhc2Div) + 1U))
179 #define BOARD_SD_HOST_BASEADDR BOARD_USDHC1_BASEADDR
180 #define BOARD_SD_HOST_CLK_FREQ BOARD_USDHC1_CLK_FREQ
181 #define BOARD_SD_HOST_IRQ USDHC1_IRQn
183 #define BOARD_MMC_HOST_BASEADDR BOARD_USDHC2_BASEADDR
184 #define BOARD_MMC_HOST_CLK_FREQ BOARD_USDHC2_CLK_FREQ
185 #define BOARD_MMC_HOST_IRQ USDHC2_IRQn
186 #define BOARD_MMC_VCCQ_SUPPLY kMMC_VoltageWindow170to195
187 #define BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360
188 /* we are using the BB SD socket to DEMO the MMC example,but the
189  * SD socket provide 4bit bus only, so we define this macro to avoid
190  * 8bit data bus test
191  */
192 #define BOARD_MMC_SUPPORT_8BIT_BUS (1U)
193 
194 #define BOARD_SD_HOST_SUPPORT_SDR104_FREQ (200000000U)
195 #define BOARD_SD_HOST_SUPPORT_HS200_FREQ (180000000U)
196 
197 /*! @brief The WIFI-QCA shield pin. */
198 #define BOARD_INITGT202SHIELD_PWRON_GPIO GPIO1 /*!< GPIO device name: GPIO */
199 #define BOARD_INITGT202SHIELD_PWRON_PORT 1U /*!< PORT device index: 1 */
200 #define BOARD_INITGT202SHIELD_PWRON_GPIO_PIN 3U /*!< PIO4 pin index: 3 */
201 #define BOARD_INITGT202SHIELD_PWRON_PIN_NAME GPIO1_3 /*!< Pin name */
202 #define BOARD_INITGT202SHIELD_PWRON_LABEL "PWRON" /*!< Label */
203 #define BOARD_INITGT202SHIELD_PWRON_NAME "PWRON" /*!< Identifier name */
204 #define BOARD_INITGT202SHIELD_PWRON_DIRECTION kGPIO_DigitalOutput /*!< Direction */
206 #define BOARD_INITGT202SHIELD_IRQ_GPIO GPIO1 /*!< GPIO device name: GPIO */
207 #define BOARD_INITGT202SHIELD_IRQ_PORT 1U /*!< PORT device index: 1 */
208 #define BOARD_INITGT202SHIELD_IRQ_GPIO_PIN 19U /*!< PIO1 pin index: 19 */
209 #define BOARD_INITGT202SHIELD_IRQ_PIN_NAME GPIO1_19 /*!< Pin name */
210 #define BOARD_INITGT202SHIELD_IRQ_LABEL "IRQ" /*!< Label */
211 #define BOARD_INITGT202SHIELD_IRQ_NAME "IRQ" /*!< Identifier name */
212 #define BOARD_INITGT202SHIELD_IRQ_DIRECTION kGPIO_DigitalInput /*!< Direction */
214 #define BOARD_INITSILEX2401SHIELD_PWRON_GPIO GPIO1 /*!< GPIO device name: GPIO */
215 #define BOARD_INITSILEX2401SHIELD_PWRON_PORT 1U /*!< PORT device index: 1 */
216 #define BOARD_INITSILEX2401SHIELD_PWRON_GPIO_PIN 9U /*!< PIO4 pin index: 9 */
217 #define BOARD_INITSILEX2401SHIELD_PWRON_PIN_NAME GPIO1_9 /*!< Pin name */
218 #define BOARD_INITSILEX2401SHIELD_PWRON_LABEL "PWRON" /*!< Label */
219 #define BOARD_INITSILEX2401SHIELD_PWRON_NAME "PWRON" /*!< Identifier name */
220 #define BOARD_INITSILEX2401SHIELD_PWRON_DIRECTION kGPIO_DigitalOutput /*!< Direction */
222 #define BOARD_INITSILEX2401SHIELD_IRQ_GPIO GPIO1 /*!< GPIO device name: GPIO */
223 #define BOARD_INITSILEX2401SHIELD_IRQ_PORT 1U /*!< PORT device index: 1 */
224 #define BOARD_INITSILEX2401SHIELD_IRQ_GPIO_PIN 11U /*!< PIO1 pin index: 11 */
225 #define BOARD_INITSILEX2401SHIELD_IRQ_PIN_NAME GPIO1_11 /*!< Pin name */
226 #define BOARD_INITSILEX2401SHIELD_IRQ_LABEL "IRQ" /*!< Label */
227 #define BOARD_INITSILEX2401SHIELD_IRQ_NAME "IRQ" /*!< Identifier name */
228 #define BOARD_INITSILEX2401SHIELD_IRQ_DIRECTION kGPIO_DigitalInput /*!< Direction */
230 /* @Brief Board accelerator sensor configuration */
231 #define BOARD_ACCEL_I2C_BASEADDR LPI2C5
232 /* Clock divider for LPI2C clock source */
233 #define BOARD_ACCEL_I2C_CLOCK_FREQ (CLOCK_GetRootClockFreq(kCLOCK_Root_Lpi2c5))
234 
235 #define BOARD_CODEC_I2C_BASEADDR LPI2C5
236 #define BOARD_CODEC_I2C_INSTANCE 5U
237 #define BOARD_CODEC_I2C_CLOCK_SOURCE_SELECT (0U)
238 #define BOARD_CODEC_I2C_CLOCK_SOURCE_DIVIDER (5U)
239 #define BOARD_CODEC_I2C_CLOCK_FREQ (24000000U)
241 /* @Brief Board CAMERA configuration */
242 #define BOARD_CAMERA_I2C_BASEADDR LPI2C6
243 #define BOARD_CAMERA_I2C_CLOCK_ROOT kCLOCK_Root_Lpi2c6
244 #define BOARD_CAMERA_I2C_CLOCK_SOURCE (1U) /* OSC24M. */
245 #define BOARD_CAMERA_I2C_CLOCK_DIVIDER (11U) /* Divider = 12, LPI2C clock frequency 2M. */
246 
247 /*! @brief The MIPI panel pins. */
248 #define BOARD_MIPI_PANEL_RST_GPIO GPIO9
249 #define BOARD_MIPI_PANEL_RST_PIN 1
250 #define BOARD_MIPI_PANEL_POWER_GPIO GPIO11
251 #define BOARD_MIPI_PANEL_POWER_PIN 16
252 /* Back light pin. */
253 #define BOARD_MIPI_PANEL_BL_GPIO GPIO9
254 #define BOARD_MIPI_PANEL_BL_PIN 29
256 /* Touch panel. */
257 #define BOARD_MIPI_PANEL_TOUCH_I2C_BASEADDR LPI2C5
258 #define BOARD_MIPI_PANEL_TOUCH_I2C_CLOCK_ROOT kCLOCK_Root_Lpi2c5
259 #define BOARD_MIPI_PANEL_TOUCH_I2C_CLOCK_SOURCE (1U) /* OSC24M. */
260 #define BOARD_MIPI_PANEL_TOUCH_I2C_CLOCK_DIVIDER (11U) /* Divider = 12, LPI2C clock frequency 2M. */
261 #define BOARD_MIPI_PANEL_TOUCH_I2C_CLOCK_FREQ CLOCK_GetRootClockFreq(BOARD_MIPI_PANEL_TOUCH_I2C_CLOCK_ROOT)
262 #define BOARD_MIPI_PANEL_TOUCH_RST_GPIO GPIO9
263 #define BOARD_MIPI_PANEL_TOUCH_RST_PIN 0
264 #define BOARD_MIPI_PANEL_TOUCH_INT_GPIO GPIO8
265 #define BOARD_MIPI_PANEL_TOUCH_INT_PIN 31
267 /*! @brief The camera pins. */
268 #define BOARD_CAMERA_PWDN_GPIO GPIO9
269 #define BOARD_CAMERA_PWDN_PIN 25
270 #define BOARD_CAMERA_RST_GPIO GPIO11
271 #define BOARD_CAMERA_RST_PIN 15
272 
273 /* SD card detection method when using wifi module. */
274 #define BOARD_WIFI_SD_DETECT_TYPE kSDMMCHOST_DetectCardByHostDATA3
276 #if defined(__cplusplus)
277 extern "C" {
278 #endif /* __cplusplus */
280 /*******************************************************************************
281  * API
282  ******************************************************************************/
283 uint32_t BOARD_DebugConsoleSrcFreq(void);
284 
285 void BOARD_InitDebugConsole(void);
286 
287 void BOARD_ConfigMPU(void);
288 #if defined(SDK_I2C_BASED_COMPONENT_USED) && SDK_I2C_BASED_COMPONENT_USED
289 void BOARD_LPI2C_Init(LPI2C_Type *base, uint32_t clkSrc_Hz);
290 status_t BOARD_LPI2C_Send(LPI2C_Type *base,
291  uint8_t deviceAddress,
292  uint32_t subAddress,
293  uint8_t subaddressSize,
294  uint8_t *txBuff,
295  uint8_t txBuffSize);
296 status_t BOARD_LPI2C_Receive(LPI2C_Type *base,
297  uint8_t deviceAddress,
298  uint32_t subAddress,
299  uint8_t subaddressSize,
300  uint8_t *rxBuff,
301  uint8_t rxBuffSize);
302 status_t BOARD_LPI2C_SendSCCB(LPI2C_Type *base,
303  uint8_t deviceAddress,
304  uint32_t subAddress,
305  uint8_t subaddressSize,
306  uint8_t *txBuff,
307  uint8_t txBuffSize);
308 status_t BOARD_LPI2C_ReceiveSCCB(LPI2C_Type *base,
309  uint8_t deviceAddress,
310  uint32_t subAddress,
311  uint8_t subaddressSize,
312  uint8_t *rxBuff,
313  uint8_t rxBuffSize);
314 void BOARD_Accel_I2C_Init(void);
315 status_t BOARD_Accel_I2C_Send(uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint32_t txBuff);
316 status_t BOARD_Accel_I2C_Receive(
317  uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
318 void BOARD_Codec_I2C_Init(void);
319 status_t BOARD_Codec_I2C_Send(
320  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, const uint8_t *txBuff, uint8_t txBuffSize);
321 status_t BOARD_Codec_I2C_Receive(
322  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
323 void BOARD_Camera_I2C_Init(void);
324 status_t BOARD_Camera_I2C_Send(
325  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, const uint8_t *txBuff, uint8_t txBuffSize);
326 status_t BOARD_Camera_I2C_Receive(
327  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
328 
329 status_t BOARD_Camera_I2C_SendSCCB(
330  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, const uint8_t *txBuff, uint8_t txBuffSize);
331 status_t BOARD_Camera_I2C_ReceiveSCCB(
332  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
333 
334 void BOARD_MIPIPanelTouch_I2C_Init(void);
335 status_t BOARD_MIPIPanelTouch_I2C_Send(
336  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, const uint8_t *txBuff, uint8_t txBuffSize);
337 status_t BOARD_MIPIPanelTouch_I2C_Receive(
338  uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
339 #endif /* SDK_I2C_BASED_COMPONENT_USED */
340 
341 void BOARD_SD_Pin_Config(uint32_t speed, uint32_t strength);
342 void BOARD_MMC_Pin_Config(uint32_t speed, uint32_t strength);
343 
344 #if defined(__cplusplus)
345 }
346 #endif /* __cplusplus */
347 
348 #endif /* _BOARD_H_ */
void BOARD_InitDebugConsole(void)
Definition: board.c:15
void BOARD_MMC_Pin_Config(uint32_t speed, uint32_t strength)
Definition: board.c:84
uint32_t BOARD_DebugConsoleSrcFreq(void)
Definition: board.c:25
void BOARD_SD_Pin_Config(uint32_t speed, uint32_t strength)
Definition: board.c:51
void BOARD_ConfigMPU(void)
Definition: board.c:52