Getting Started with Zephyr (MCXN947)

Hardware Requirements

These labs are written for the evaluation board listed below. However, these labs use sample applications in the Zephyr repository, and will easily run on other NXP boards supported in the Zephyr tree:

  • FRDM-MCXN947

  • USB Type-C cable

  • This board integrates an on-board debugger, and the labs are written to use this debugger with the default MCU-Link CMSIS-DAP debug probe.

    FRDM-MCXN947

Zephyr Lab Guides with VS Code

This set of lab guides provide detailed steps to get started with Zephyr and the MCUXpresso extension for VS Code using the FRDM-MCXN947 board:

Lab Notes

  • The lab steps are written for Windows 11. But Zephyr and NXP’s tools, including the MCUXpresso extension for VS Code, are also supported on Ubuntu and macOS. All the labs will work on each supported OS with minimal changes needed.