This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

How to add or remove boot header for XIP targets

The MCUXpresso SDK for i.MX RT1170 provides flexspi_nor_debug and flexspi_nor_release targets for each example and/or demo which supports XIP (eXecute-In-Place). These two targets add XIP_BOOT_HEADER to the image by default. Because of this, ROM can boot and run this image directly on external flash.

Macros for the boot leader:

  • The following three macros are added in flexspi_nor targets to support XIP, as described in Table 1.

    |XIP_​EXTERNAL_​FLASH|1: Exclude the code which changes the clock of FLEXSPI.​| |0: Make no changes.​| |XIP_​BOOT_​HEADER_​ENABLE|1: Add FLEXSPI configuration block, image vector table, boot data, and device configuration data (optional) to the image by default.​| |0: Add nothing to the image by default.​| |XIP_​BOOT_​HEADER_​DCD_​ENABLE|1: Add device configuration data to the image.​| |0: Do NOT add device configuration data to the image.​|

  • Table 2 shows the different effect on the built image with a different combination of these macros.

    XIP_​BOOT_​HEADER_​DCD_​ENABLE=1

    XIP_​BOOT_​HEADER_​DCD_​ENABLE=0

    XIP_​EXTERNAL_​FLASH=1

    XIP_​BOOT_​HEADER_​ENABLE=1

    - Can be programmed to qspiflash by IDE and can run after POR reset if qspiflash is the boot source.​

    • SDRAM will be initialized.​ | - Can be programmed to qspiflash by IDE, and can run after POR reset if qspiflash is the boot source.​

    • SDRAM will NOT be initialized.​ | |XIP_​BOOT_​HEADER_​ENABLE=0| - CANNOT run after POR reset if it is programmed by IDE, even if qspiflash is the boot source.​ |—| |XIP_​EXTERNAL_​FLASH=0| - This image CANNOT complete XIP because when this macro is set to 1, it excludes the code, which changes the clock for FLEXSPI.​ |

Where to change the macros for each toolchain in MCUXpresso SDK?

Take hello_world as an example:

  • IAR

  • MDK

  • ARMGCC

    Change the configuration in CMakeLists.txt.

  • MCUX