This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

MISRA compliance

All MCUXpresso SDK drivers comply to MISRA 2012 rules with exceptions in Table 1.

|Exception rules

|Description

| |—————–|————-| |Directive 4.​4

|Sections of code should not be commented out.​

| |Directive 4.​5

|Identifiers in the same namespace with overlapping visibility should be typographically unambiguous.​

| |Directive 4.​6

|Typedefs that indicate size and signedness should be used in place of the basic numerical types.​

| |Directive 4.​8

|If a pointer to a structure or union is never dereferenced within a translation unit, then the implementation of the object should be hidden.​

| |Directive 4.​9

|A function should be used in preference to a function-​like macro where they are interchangeable.​

| |Directive 4.​13

|Functions which are designed to provide operations on a resource should be called in an appropriate sequence.​

| |Rule 1.​2

|Language extensions should not be used.​

| |Rule 2.​3

|A project should not contain unused type declarations.​

| |Rule 2.​4

|A project should not contain unused tag declarations.​

| |Rule 2.​5

|A project should not contain unused macro declarations.​

| |Rule 2.​6

|A function should not contain unused label declarations.​

| |Rule 2.​7

|There should be no unused parameters in functions.​

| |Rule 4.​2

|Trigraphs should not be used.​

| |Rule 5.​1

|External identifiers shall be distinct.​

| |Rule 5.​4

|Macro identifiers shall be distinct.​

| |Rule 5.​9

|Identifiers that define objects or functions with internal linkage should be unique.​

| |Rule 8.​7

|Functions and objects should not be defined with external linkage if they are referenced in only one translation unit.​

| |Rule 8.​9

|An object should be defined at block scope if its identifier only appears in a single function.​

| |Rule 8.​11

|When an array with external linkage is declared, its size should be explicitly specified.​

| |Rule 8.​13

|A pointer should point to a const-​qualified type whenever possible.​

| |Rule 10.​5

|The value of an expression should not be cast to an inappropriate essential type.​

| |Rule 11.​4

|A conversion should not be performed between a pointer to object and an integer type.​

| |Rule 11.​5

|A conversion should not be performed from pointer to void into pointer to object.​

| |Rule 12.​1

|The precedence of operators within expressions should be made explicit.​

| |Rule 12.​3

|The comma operator should not be used.​

| |Rule 12.​4

|Evaluation of constant expressions should not lead to unsigned integer wrap-​around.​

| |Rule 13.​3

|A full expression containing an increment (++) or decrement (–) operator should have no other potential side effects other than that caused by the increment or decrement operator.​

| |Rule 15.​4

|There should be no more than one break or go to statement used to terminate any iteration statement.​

| |Rule 17.​5

|The function argument corresponding to a parameter declared to have an array type shall have an appropriate number of elements.​

| |Rule 17.​8

|A function parameter should not be modified.​

| |Rule 19.​2

|The union keyword should not be used.​

| |Rule 20.​1

|#include directives should only be preceded by preprocessor directives or comments.​

| |Rule 20.​10

|The # and ## preprocessor operators should not be used.​

| |Rule 21.​1

|#define and #undef shall not be used on a reserved identifier or reserved macro name.​

| |Rule 21.​2

|A reserved identifier or macro name shall not be declared.​

| |Rule 21.​12

|The exception handling features of <fenv.​h> should not be used.​

|