Run a demo application using IAR
Build an example application
Do the following steps to build the hello_world
example application.
Open the desired demo application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
Using the EVK-MIMXRT1024 hardware platform as an example, the
hello_world
workspace is located in:<install_dir>/boards/evkmimxrt1024/demo_apps/hello_world/iar/hello_world.eww
Other example applications may have additional folders in their path.
Select the desired build target from the drop-down menu.
There are twelve project configurations (build targets) supported for most MCUXpresso SDK projects:
Debug
– Compiler optimization is set to low, and debug information is generated for the executable. The linker file isRAM
linker, where text and data section is put in internal TCM.Release
– Compiler optimization is set to high, and debug information is not generated. The linker file isRAM
linker, where text and data section is put in internal TCM.ram_0x1400_debug
– Project configuration is same as the debug target. The linker file isRAM_0x1400
linker, where text is put in ITCM with offset 0x1400 and data put in DTCM.ram_0x1400_release
– Project configuration is same as the release target. The linker file isRAM_0x1400
linker, where text is put in ITCM with offset 0x1400 and data put in DTCM.sdram_debug
– Project configuration is same as the debug target. The linker file isSDRAM
linker, where text is put in internal TCM and data put in SDRAM.sdram_release
– Project configuration is same as the release target. The linker file isSDRAM
linker, where text is put in internal TCM and data put in SDRAM.sdram_txt_debug
– Project configuration is same as the debug target. The linker file isSDRAM_txt
linker, where text is put in SDRAM and data put in OCRAM.sdram_txt_release
– Project configuration is same as the release target. The linker file isSDRAM_txt
linker, where text is put in SDRAM and data put in OCRAM.flexspi_nor_debug
– Project configuration is same as the debug target. The linker file isflexspi_nor
linker, where text is put in flash and data put in TCM.flexspi_nor_release
– Project configuration is same as the release target. The linker file isflexspi_nor
linker, where text is put in flash and data put in TCM.flexspi_nor_sdram_release
- Project configuration is same as the release target. The linker file isflexspi_nor_sdram
linker, where text is put in flash and data put in SDRAM.flexspi_nor_sdram_debug
– Project configuration is same as the debug target. The linker file isflexspi_nor_sdram
linker, where text is put in flash and data put in SDRAM. For some examples need large data memory, onlysdram_debug
andsdram_release
targets are supported.
For this example, select hello_world – debug.
|
|
To build the demo application, click Make, highlighted in red in Figure 2.
|
|
The build completes without errors.
Parent topic:Run a demo application using IAR
Run an example application
To download and run the application, perform these steps:
This board supports the CMSIS-DAP/mbed/DAPLink debug probe by default. Visit os.mbed.com/handbook/Windows-serial-configuration and follow the instructions to install the Windows operating system serial driver. If running on Linux OS, this step is not required.
Connect the development platform to your PC via USB cable. Connect the USB cable to J41 and make sure SW7[1:4] is 0010b.
Open the terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug COM port (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:
115200 or 9600 baud rate, depending on your board (reference
BOARD_DEBUG_UART_BAUDRATE
variable in theboard.h
file)No parity
8 data bits
1 stop bit
|
|
In IAR, click the Download and Debug button to download the application to the target.
|
|
When using jlink to debug debug/release targets on IAR, an extra option is specified in debugger settings. Check **Debugger \> Extra Options \> Command-line** options and fill the following contents: `--jlink_script_file=$PROJ_DIR$/../evkmimxrt1024_sdram_init.jlinkscript`.
The application is then downloaded to the target and automatically runs to the
main()
function.|
|
Run the code by clicking the Go button to start the application.
|
|
The
hello_world
application is now running and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.|
|
Parent topic:Run a demo application using IAR