This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

MCUXpresso configuration tools

MCUXpresso Config Tools can help configure the processor and generate initialization code for the on-chip peripherals. The tools are able to modify any existing example project, or create a configuration for the selected board or processor. The generated code is used with MCUXpresso SDK version 2.x.

Table 1 describes the tools included in the MCUXpresso config tools.

Config tool

Description

Image

Pins tool

For configuration of pin routing and pin electrical properties.​

Clock tool

For system clock configuration.​

Peripherals tools

For configuration of other peripherals

TEE tool

Configures access policies for memory area and peripherals helping to protect and isolate sensitive parts of the application.​

MCUXpresso Config Tools can be accessed in the following products:

  • Integrated in the MCUXpresso IDE. Config tools are integrated with both compiler and debugger which makes it the easiest way to begin the development.

  • Standalone version available for download from MCUXPRESSO. Recommended for customers using IAR Embedded Workbench, Keil MDK µVision, or Arm GCC.

  • Online version available on MCUXPRESSO. Recommended ding a quick evaluation of the processor or use the tool without installation.

Each version of the product contains a specific Quick Start Guide document MCUXpresso IDE Config Tools installation folder that can help start your work.