This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Run and Debug from Command-Line Environment / LINUX

RT600 SDK has been configured to be as flexible to support multiple toolchains, including the Arm GCC and XCC command-line environments. The principles and essentials are still the same as with the IDE. The command-line environment settings are nearly identical between WIN32 and LINUX, with few different path settings.

Build and Debug Arm Application

The Arm application requires the GNU Arm Embedded Toolchain and CMake version 3.x for command-line compile and linking. For more information on installation and configuration of required build tools for command-line development, see the Getting Started with MCUXpresso SDK for EVK_MIMXRT685.pdf in the <SDK_ROOT>/docs/ directory.

To build and debug:

  1. Launch a command prompt / terminal and change directory to the xaf_record application.

    user@linux:~/SDK/boards/evkmimxrt685/dsp_examples/xaf_record/cm33/armgcc$ ls -1
    build_all.bat
    build_all.sh
    build_debug.bat
    build_debug.sh
    build_flash_debug.bat
    build_flash_debug.sh
    build_flash_release.bat
    build_flash_release.sh
    build_release.bat
    build_release.sh
    clean.bat
    clean.sh
    CMakeLists.txt
    
  2. Use .bat files to build the configuration on Windows, and .sh files on Linux/UNIX.

    user@linux:~/SDK/boards/evkmimxrt685/dsp_examples/xaf_record/cm33/armgcc$ ./build_debug.sh
    ...
    [100%] Linking C executable debug/dsp_xaf_record_cm33.elf
    [100%] Built target dsp_xaf_record_cm33.elf
    
  3. Launch the GDB server.

    user@linux:/opt/JLink$ ./JLinkGDBServerCLExe -device MIMXRT685S_M33 -if SWD
    SEGGER J-Link GDB Server V6.46j Command Line Version
    ...
    Listening on TCP/IP port 2331
    Connecting to target...Connected to target
    Waiting for GDB connection...
    
  4. Connect with GDB to the device and load Arm application.

    user@jlinux:~/SDK/boards/evkmimxrt685/dsp_examples/xaf_record/cm33/armgcc$ arm-none-eabi-gdb debug/dsp_xaf_record_cm33.elf
    ...
    Reading symbols from debug/dsp_xaf_record_cm33.elf...
    (gdb) target remote localhost:2331
    Remote debugging using localhost:2331
    0x1301ec7a in ?? ()
    (gdb) mon reset
    Resetting target
    (gdb) load
    Loading section .flash_config, size 0x200 lma 0x7f400
    Loading section .interrupts, size 0x130 lma 0x80000
    Loading section .text, size 0xe330 lma 0x80130
    Loading section CodeQuickAccess, size 0x52c lma 0x8e460
    Loading section .ARM, size 0x8 lma 0x8e98c
    Loading section .init_array, size 0x4 lma 0x8e994
    Loading section .fini_array, size 0x4 lma 0x8e998
    Loading section .data, size 0x104 lma 0x8e99c
    Start address 0x801e4, load size 60576
    Transfer rate: 272 KB/sec, 5506 bytes/write.
    (gdb) b main
    Breakpoint 1 at 0x808f2: file /SDK/boards/src/dsp_examples/xaf_record/cm33/main_cm33.c, line 161.
    (gdb) c
    Continuing.
    Breakpoint 1, main ()
        at /SDK/boards/src/dsp_examples/xaf_record/cm33/main_cm33.c:161
    161     BOARD_InitHardware();
    

Parent topic:Run and Debug from Command-Line Environment / LINUX

Build and Debug DSP Application

The Xtensa command-line toolchain is installed as part of the Xplorer IDE. The tools can be optionally installed on a new Windows or Linux system without the IDE using the redistributable compressed file found at: <XTENSA_ROOT>/XtDevTools/downloads/RI-2023.11/tools/. For more information, see Install Xtensa On Chip Debugger Daemon.

In order to use the command-line tools, some environment variables must be set up for use with the cmake build scripts:

# Add tools binaries to PATH.  Assume ~/xtensa/ is install root - please adjust accordingly.
export PATH=$PATH:~/xtensa/XtDevTools/install/tools/RI-2023.11-linux/XtensaTools/bin
# (Optional) Use environment variable to control license file
# NOTE: ~/.flexlmrc will override this selection.  Please delete that file before proceeding.
export LM_LICENSE_FILE=~/RT600.lic
# Setup env vars needed for compile and linking
export XCC_DIR=~/xtensa/XtDevTools/install/tools/RI-2023.11-linux/XtensaTools
export XTENSA_SYSTEM=~/xtensa/XtDevTools/install/builds/RI-2023.11-linux/
nxp_rt600_RI23_11_newlib/configexport XTENSA_CORE=nxp_rt600_RI23_11_newlibb

Note: On Windows, you can use the ‘setx’ command instead of the ‘export’ command to set the environment variables.

  1. Use the batch/shell script to build out the DSP application from the command line, in the ‘xcc’ directory:

    user@linux:~/SDK/boards/evkmimxrt685/dsp_examples/xaf_record/dsp/xcc$ ./build_debug.sh
    ...
    [100%] Built target dsp_xaf_record_hifi4.elf
    

    Note: Some warnings during the linking process (floating-point ABI) may appear. However, the warnings may be ignored.

  2. Launch xt-ocd debugging server (replace topology.xml with your custom version – see section 1.5 of this document):

    user@linux:/opt/Tensilica/xocd-14.11$ ./xt-ocd.exe -c topology.xml
    

    Note: If the Arm core fails to initialize the DSP, the xt-ocd daemon may fail to start. Therefore, the Arm core must initialize the DSP first.

  3. Connect with Xtensa GDB to the device and execute the DSP application:

    user@linux:/SDK/boards/evkmimxrt685/dsp_examples/xaf_record/dsp/xcc$ xt-gdb
    debug/dsp_xaf_record_hifi4.elf
    GNU gdb (GDB) 7.11.1 <Xtensa Tools VERSION NUMBER>
    ...
    Reading symbols from debug/dsp_xaf_record_hifi4.elf...done.
    (xt-gdb)
    (xt-gdb) target remote localhost:20000
    Remote debugging using localhost:20000
    _DoubleExceptionVector ()
        at /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xos/src/xos_vectors.S:216
    216 /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xos/src/xos_vectors.S: No such file or directory.
    (xt-gdb) reset
    _ResetVector ()
        at /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xtos/xea2/reset-vector-xea2.S:71
    71  /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux/xtensa-elf/src/xtos/xea2/reset-vector-xea2.S: No such file or directory.
    (xt-gdb) load
    Loading section .rtos.rodata, size 0x80 lma 0x200000
    Loading section .rodata, size 0x17d50 lma 0x200080
    Loading section .text, size 0x633f0 lma 0x217dd0
    Loading section .rtos.percpu.data, size 0x4 lma 0x27b1c0
    Loading section .data, size 0x110c lma 0x27b1d0
    Loading section NonCacheable, size 0x2960 lma 0x20040000
    Loading section .Level3InterruptVector.literal, size 0x4 lma 0x24000000
    Loading section .DebugExceptionVector.literal, size 0x4 lma 0x24000004
    Loading section .NMIExceptionVector.literal, size 0x4 lma 0x24000008
    Loading section .ResetVector.text, size 0x13c lma 0x24020000
    Loading section .WindowVectors.text, size 0x16c lma 0x24020400
    Loading section .Level2InterruptVector.text, size 0x1c lma 0x2402057c
    Loading section .Level3InterruptVector.text, size 0xc lma 0x2402059c
    Loading section .DebugExceptionVector.text, size 0xc lma 0x240205bc
    Loading section .NMIExceptionVector.text, size 0xc lma 0x240205dc
    Loading section .KernelExceptionVector.text, size 0xc lma 0x240205fc
    Loading section .UserExceptionVector.text, size 0x18 lma 0x2402061c
    Loading section .DoubleExceptionVector.text, size 0x8 lma 0x2402063c
    Start address 0x24020000, load size 520016
    Transfer rate: 8 KB/sec, 10612 bytes/write.
    (xt-gdb) b main
    Breakpoint 1 at 0x21ab5b: file /SDK/boards/src/dsp_examples/xaf_record/hifi4/xaf_main_hifi4.c, line 366.
    (xt-gdb) c
    Continuing.
    Breakpoint 1, main ()
        at /SDK/boards/src/dsp_examples/xaf_record/hifi4/xaf_main_hifi4.c:366
    366     xos_start_main("main", 7, 0);
    (xt-gdb) c
    Continuing.
    

    Note: You can use the gdb command ‘set substitute-path’ to map the missing symbols from the toolchain libraries. For example:

    set substitute-path /home/xpgcust/tree/RI-2023.11/ib/tools/swtools-x86_64-linux ~/xtensa/tools/RI-2023.11-linux/XtensaTools
    

    For more information on xt-gdb, see the Cadence GNU Debugger User’s Guide and the Cadence Xtensa Debug Guide. The documents are available at:

    • ~/xtensa/XtDevTools/downloads/RI-2023.11/docs/gnu_gdb_ug.pdf

    • ~/xtensa/XtDevTools/downloads/RI-2023.11/docs/xtensa_debug_guide.pdf

Parent topic:Run and Debug from Command-Line Environment / LINUX