This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Default debug interfaces

The MCUXpresso SDK supports various hardware platforms that come loaded with a variety of factory programmed debug interface configurations. Table 1 lists the hardware platforms supported by the MCUXpresso SDK, their default debug interface, and any version information that helps differentiate a specific interface configuration.

Note: The OpenSDA details column is not applicable to LPC.

Hardware platform

Default interface

OpenSDA details

FRDM-KE17Z

CMSIS-DAP/mbed/DAPLink

OpenSDA v2.2