This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Known Issues

This section lists the known issues, limitations, and/or workarounds.

Maximum file path length in Windows 7 operating system

The Windows 7 operating system imposes a 260-character maximum length for file paths. When installing the MCUXpresso SDK, place it in a directory close to the root to prevent file paths from exceeding the maximum character length specified by the Windows operating system. The recommended location is the C:\<folder>.

Parent topic:Known Issues

eDMA examples accessing AIPS peripheral bridge memory must run through U-Boot loading method

Non-secure access to Arm IP Bus (AIPS) must be configured in Trusted Resource Domain Control (TRDC) for enhanced direct memory access (eDMA) controller. Due to the limitation that Sentinel ROM can release TRDC only once, such examples must run through U-Boot loading method after Trusted Firmware-A (TF-A) configuring TRDC.

To make low-power boot mode work for only M core in such example, you need to implement the request of the TRDC release and configure TRDC. However, it will break the single boot mode with TF-A/Linux BSP.

The following eDMA examples need access to AIPS.

  • cmsis_lpi2c_edma_b2b_transfer_master

  • cmsis_lpi2c_edma_b2b_transfer_slave

  • cmsis_lpuart_edma_transfer

  • flexcan_loopback_edma_transfer

  • lpi2c_edma_b2b_transfer_master

  • lpi2c_edma_b2b_transfer_slave

  • lpuart_edma_transfer

  • pdm_edma_transfer

  • sai_edma_transfer

Parent topic:Known Issues